Hi
I would like to run the H264 Decoder on Core 0 and the H264 Encoder on Core 1 of the C6657
I am using H264HPDEC 1.1.6.0 and H264HPENC 1.0.3.0
I am trying to use the same build running on both cores using DNUM at runtime.
Is this possible with these prebuilt libraries? I have no problems running them at the same time on core0 but initializing one core seems to interfere with the other core.
Thanks
Dhar