This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2HG: CPU [IPU1-0 ] Statistics

Part Number: TDA2HG

Hello,

We need to get the CPU Statistics of IPU1_0. However, it can not print this with function of ChainsCommon_printCpuStatus.

Thanks

Terence

=============================================================================

[HOST] [IPU2 ] 101.221923 s: CPU [IPU1-0 ] Statistics,
[HOST] [IPU2 ] 101.221984 s: *************************
[HOST] [IPU2 ] 101.222045 s: CPU: IPU1-0: Unable to get CPU statistics !!!
[HOST] [IPU2 ] 101.222320 s:
[HOST] [IPU2 ] 101.222381 s:
[HOST] [IPU2 ] 101.222442 s:
[HOST] [IPU2 ] 101.222473 s: CPU [DSP1 ] Statistics,
[HOST] [IPU2 ] 101.222534 s: *************************
[HOST] [IPU2 ] 101.222595 s:
[HOST] [IPU2 ] 101.222656 s: LOAD: CPU: 0.3% HWI: 0.1%, SWI:0.0%, Low Power: 97.4%
[HOST] [IPU2 ] 101.222839 s:
[HOST] [IPU2 ] 101.222900 s: LOAD: TSK: MISC : 0.2%
[HOST] [IPU2 ] 101.222961 s:
[HOST] [IPU2 ] 101.223022 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023
[HOST] [IPU2 ] 101.223113 s:
[HOST] [IPU2 ] 101.223144 s: SYSTEM: Sempahores Objects, 456 of 1050 free
[HOST] [IPU2 ] 101.223235 s: SYSTEM: Task Objects , 91 of 100 free
[HOST] [IPU2 ] 101.223327 s: SYSTEM: Clock Objects , 99 of 100 free
[HOST] [IPU2 ] 101.223418 s: SYSTEM: Hwi Objects , 100 of 100 free
[HOST] [IPU2 ] 101.223510 s:
[HOST] [IPU2 ] 101.223540 s: SYSTEM: Heap = LOCAL_L2 @ 0x00800000, Total size = 227264 B (221 KB), Free size = 227264 B (221 KB)
[HOST] [IPU2 ] 101.223723 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 524288 B (512 KB), Free size = 517128 B (505 KB)
[HOST] [IPU2 ] 101.223906 s:
[HOST] [IPU2 ] 101.223937 s:
[HOST] [IPU2 ] 101.223967 s: CPU [DSP2 ] Statistics,
[HOST] [IPU2 ] 101.224028 s: *************************
[HOST] [IPU2 ] 101.224089 s:
[HOST] [IPU2 ] 101.224150 s: LOAD: CPU: 0.3% HWI: 0.1%, SWI:0.0%, Low Power: 97.4%
[HOST] [IPU2 ] 101.224272 s:
[HOST] [IPU2 ] 101.224333 s: LOAD: TSK: MISC : 0.2%
[HOST] [IPU2 ] 101.224425 s:
[HOST] [IPU2 ] 101.224455 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023
[HOST] [IPU2 ] 101.224547 s:
[HOST] [IPU2 ] 101.224608 s: SYSTEM: Sempahores Objects, 456 of 1050 free
[HOST] [IPU2 ] 101.224669 s: SYSTEM: Task Objects , 91 of 100 free
[HOST] [IPU2 ] 101.224791 s: SYSTEM: Clock Objects , 99 of 100 free
[HOST] [IPU2 ] 101.224882 s: SYSTEM: Hwi Objects , 100 of 100 free
[HOST] [IPU2 ] 101.224974 s:
[HOST] [IPU2 ] 101.225004 s: SYSTEM: Heap = LOCAL_L2 @ 0x00800000, Total size = 227264 B (221 KB), Free size = 227264 B (221 KB)
[HOST] [IPU2 ] 101.225187 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 524288 B (512 KB), Free size = 517128 B (505 KB)