This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Brightness control on AM3715EVM



Hi,

 

I am wondering whether brightness control is actually functional on AM3715evm running FroYo. The GUI appears to be functional  (I can move the slider to increase/decrease brightness) but it has no effect on actual brightness of the screen. Is it supposed to be working? Does HW support exist?

 

Thanks,

Michael

  • Hi Michael,

    Brightness control is not functional on AM3517evm running on froyo. This is because HW does not support brightness control.

    HW supports only OFF(Disable LCD) and ON(Enable LCD).

    echo 4 > /sys/class/graphics/fb0/blank disables LCD.

    echo 0 > /sys/class/graphics/fb0/blank enables LCD.

    Regards,

    Arun