Part Number: 66AK2H12
Hy,
We made some progress with our Hyperlink testing on custom board. The hyperlink LLD example program can run successfully on both device in non-loopback mode. The question related to this was:
I've ran the mpm-transport library tests and they finished successfully. The mpm_transport_hyplnk_remote.out program uses hyperlink-0 as default port. I modified it to use hyperlink-1 on one DSP. Each port is functioning properly, according to the testprogram. The program trace is the following:
testing hyperlink mmap write
completed hyperlink mmap read and check
testing hyperlink mpm_transport_write and mpm_transport_read
Testing remote 36-bit put
Testing remote interrupt
Waiting for interrupt.2..with 5 sec timeout
wait for interrupt 2 timed out
Thread 1 created successfully
Thread: Waiting for interrupt.3..
Thread 2 created successfully
Thread: Waiting for interrupt.3 A..
Thread 3 created successfully
Background loop 1 executing...
Thread: Waiting for interrupt.3 B..
Generating test interrupt from background
Background loop 1 executing...
Thread: Wait for interrupt 3 A complete , event bitmap c result: 1
Thread: Wait for interrupt 3 complete , event bitmap 4 result: 1
Background loop 3 executing...
Thread: Wait for interrupt 3 B complete , event bitmap 2 result: 1
Testing remote interrupt: using model 2
Waiting for interrupt.4..with 5 sec timeout
Interrupt 4 wait timed out
mpm transport: hyperlink remote test passed
Our goal is to run ti-openmpi nbody testprogram successfully over hyperlink. The testmpi program is also successful. Only nbody fails. The verbose trace of the nbody is the following:
/opt/ti-openmpi/bin/mpirun --mca btl_base_verbose 100 --mca btl self,hlink -np 2 -host DSP1,DSP2 ./nbody 1000
[DSP2:02204] mca: base: components_open: Looking for btl components [DSP2:02204] mca: base: components_open: opening btl components [DSP2:02204] mca: base: components_open: found loaded component hlink [DSP2:02204] BTL_HLINK TIMPIDBG: hlink_component_register!!! [DSP2:02204] This is EVM, using hl0 only! [DSP2:02204] mca: base: components_open: component hlink register function successful [DSP2:02204] BTL_HLINK TIMPIDBG: hlink_component_open!!! [DSP2:02204] BTL_HLINK BTL HLINK start of HYPLNKINITCFG: 0xb6a70130 [DSP2:02204] BTL_HLINK [0x21400000] [DSP2:02204] BTL_HLINK [0x40000000] [DSP2:02204] BTL_HLINK [0x21400100] [DSP2:02204] BTL_HLINK [0x28000000] [DSP2:02204] BTL_HLINK [(nil)] [DSP2:02204] BTL_HLINK [(nil)] [DSP2:02204] BTL_HLINK [(nil)] [DSP2:02204] BTL_HLINK [(nil)] [DSP2:02204] BTL_HLINK BTL HLINK end of HYPLNKINITCFG [DSP2:02204] BTL_HLINK: CMEM_init OK! [DSP2:02204] mca: base: components_open: component hlink open function successful [DSP2:02204] mca: base: components_open: found loaded component self [DSP2:02204] mca: base: components_open: component self has no register function [DSP2:02204] mca: base: components_open: component self open function successful [DSP1:02191] mca: base: components_open: Looking for btl components [DSP2:02204] select: initializing btl component hlink [DSP2:02204] BTL_HLINK TIMPIDBG: hlink_component_init!!! [DSP2:02204] BTL_HLINK shmem open successfull!! [DSP2:02204] BTL_HLINK: CMEM physAddr: 22000000 (to a2000000) userAddr:0xb5989000 [DSP2:02204] BTL_HLINK shmem MSMC0 mmap successfull!! [DSP2:02204] BTL_HLINK shmem MSMC0 mmap successfull!! [DSP2:02204] BTL_HLINK attempt HyperLink0 then HyperLink1 [DSP2:02204] BTL_HLINK hyplnk0 attempt opening [DSP2:02204] BTL_HLINK hyplnk0 open successfull!! [DSP2:02204] BTL_HLINK hyplnk1 attempt opening [DSP1:02191] mca: base: components_open: opening btl components [DSP1:02191] mca: base: components_open: found loaded component hlink [DSP1:02191] BTL_HLINK TIMPIDBG: hlink_component_register!!! [DSP1:02191] This is EVM, using hl0 only! [DSP1:02191] mca: base: components_open: component hlink register function successful [DSP1:02191] BTL_HLINK TIMPIDBG: hlink_component_open!!! [DSP1:02191] BTL_HLINK BTL HLINK start of HYPLNKINITCFG: 0xb6a1a130 [DSP1:02191] BTL_HLINK [0x21400000] [DSP1:02191] BTL_HLINK [0x40000000] [DSP1:02191] BTL_HLINK [0x21400100] [DSP1:02191] BTL_HLINK [0x28000000] [DSP1:02191] BTL_HLINK [(nil)] [DSP1:02191] BTL_HLINK [(nil)] [DSP1:02191] BTL_HLINK [(nil)] [DSP1:02191] BTL_HLINK [(nil)] [DSP1:02191] BTL_HLINK BTL HLINK end of HYPLNKINITCFG [DSP1:02191] BTL_HLINK: CMEM_init OK! [DSP1:02191] mca: base: components_open: component hlink open function successful [DSP1:02191] mca: base: components_open: found loaded component self [DSP1:02191] mca: base: components_open: component self has no register function [DSP1:02191] mca: base: components_open: component self open function successful [DSP1:02191] select: initializing btl component hlink [DSP1:02191] BTL_HLINK TIMPIDBG: hlink_component_init!!! [DSP1:02191] BTL_HLINK shmem open successfull!! [DSP1:02191] BTL_HLINK: CMEM physAddr: 22000000 (to a2000000) userAddr:0xb5933000 [DSP1:02191] BTL_HLINK shmem MSMC0 mmap successfull!! [DSP1:02191] BTL_HLINK shmem MSMC0 mmap successfull!! [DSP1:02191] BTL_HLINK attempt HyperLink0 then HyperLink1 [DSP1:02191] BTL_HLINK hyplnk0 attempt opening [DSP2:02204] BTL_HLINK hyplnk1 open failed [DSP2:02204] BTL_HLINK hyplnk0=0x77cf0 hyplnk1=(nil) [DSP2:02204] BTL_HLINK hyplnk0 MSMC mmap successfull!! [DSP2:02204] BTL_HLINK hyplnk0 DDR mmap successfull!! [DSP2:02204] BTL_HLINK BTL HLINK turned ON (hl0=1 hl1=0)!!! [DSP2:02204] select: init of component hlink returned success [DSP2:02204] select: initializing btl component self [DSP2:02204] select: init of component self returned success [DSP1:02191] BTL_HLINK hyplnk0 open failed [DSP1:02191] BTL_HLINK hyplnk1 attempt opening [DSP1:02191] BTL_HLINK hyplnk1 open successfull!! [DSP1:02191] BTL_HLINK hyplnk0=(nil) hyplnk1=0x76f38 [DSP1:02191] BTL_HLINK hyplnk1 MSMC mmap successfull!! [DSP1:02191] BTL_HLINK hyplnk1 DDR mmap successfull!! [DSP1:02191] BTL_HLINK BTL HLINK turned ON (hl0=0 hl1=1)!!! [DSP1:02191] select: init of component hlink returned success [DSP1:02191] select: initializing btl component self [DSP1:02191] select: init of component self returned success [DSP1:02191] TIMPIDBG 0 rmt_msgbase=0x9dd0b000 loc_msgbase=0xb6133000 [DSP1:02191] TIMPIDBG B hlink_module_add_procs(0) remote hostname=DSP1 (over HL0:NOTUSED HL1:DSP2, bridge:NOTUSED) rem_rank[0] jobid=c5460001 [DSP1:02191] TIMPIDBG B hlink_module_add_procs(1) remote hostname=DSP2 (over HL0:NOTUSED HL1:DSP2, bridge:NOTUSED) rem_rank[1] jobid=c5460001 [DSP2:02204] TIMPIDBG 0 rmt_msgbase=0xa5d69000 loc_msgbase=0xb5d89000 [DSP2:02204] TIMPIDBG B hlink_module_add_procs(0) remote hostname=DSP1 (over HL0:DSP1 HL1:NOTUSED, bridge:NOTUSED) rem_rank[0] jobid=c5460001 [DSP2:02204] HLINK0: TIMPIDBG[0, nlocal 0] hlink_module_add_procs, I can talk to rank: (0) on DSP1 [DSP2:02204] TIMPIDBG B hlink_module_add_procs(1) remote hostname=DSP2 (over HL0:DSP1 HL1:NOTUSED, bridge:NOTUSED) rem_rank[1] jobid=c5460001 [DSP2:02204] TIMPIDBG hlink_module_add_procs, RANKS: my_rank=1 nprocs=2 nlocal_procs=1 endpoint_count=2 [DSP1:02191] HLINK1: TIMPIDBG[1, nlocal 0] hlink_module_add_procs, I can talk to rank: (1) on DSP2 [DSP1:02191] TIMPIDBG hlink_module_add_procs, RANKS: my_rank=0 nprocs=2 nlocal_procs=1 endpoint_count=2 [DSP1:02191] TIMPIDBG: hlink_module_prepare_src EAGER: 130048 MAX: 131072 (btl=0xb6ac72fc) [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x7f900 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x7f980 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x7fa00 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x7fa80 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x7fb00 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x7fb80 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x7fc00 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x7fc80 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x7fd00 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x7fd80 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x7fe00 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x7fe80 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x7ff00 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x7ff80 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80000 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80080 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80100 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80180 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80200 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80280 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80300 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80380 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80400 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80480 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80500 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80580 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80600 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80680 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80700 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80780 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80800 [DSP1:02191] BTL HLINK fragmentInitialized (btl=0xb6ac72fc) frag=0x80880 [DSP1:02191] TIMPIDBG: hlink_module_send frag=0x80880 (base=0x9d8b848c size=28014)!!! [DSP1:02191] TIMPIDBG: hlink_module_send FIFO_WRITE: nprocs 1(0)->0, frag_hdr=0x9d8b8480 eager_limit=130048 [DSP1:02191] TMPIDBG: rmt_ep 0 send (hyplnk_iface1) (bridging 0) (use_edma 1 seg_len 28014 eager_limit 130048) [DSP1:02191] BTL_HL[ 122.505225] mpirun invoked oom-killer: gfp_mask=0x200da, order=0, oom_score_adj=0 [ 122.512698] CPU: 3 PID: 2189 Comm: mpirun Tainted: G O 3.10.72-gca334de #1 [ 122.520431] [<c00159c0>] (unwind_backtrace+0x0/0xf8) from [<c0011abc>] (show_stack+0x10/0x14) [ 122.528947] [<c0011abc>] (show_stack+0x10/0x14) from [<c05076a0>] (dump_header.isra.14+0x78/0x198) [ 122.531444] syslog-ng: page allocation failure: order:0, mode:0x201db [ 122.531449] CPU: 0 PID: 2046 Comm: syslog-ng Tainted: G O 3.10.72-gca334de #1 [ 122.531464] [<c00159c0>] (unwind_backtrace+0x0/0xf8) from [<c0011abc>] (show_stack+0x10/0x14) [ 122.531475] [<c0011abc>] (show_stack+0x10/0x14) from [<c009db40>] (warn_alloc_failed+0xa8/0x120) [ 122.531485] [<c009db40>] (warn_alloc_failed+0xa8/0x120) from [<c00a0a60>] (__alloc_pages_nodemask+0x614/0x8c8) [ 122.531492] [<c00a0a60>] (__alloc_pages_nodemask+0x614/0x8c8) from [<c009b7b0>] (filemap_fault+0x1c8/0x410) [ 122.535890] 3367 reserved pages [ 122.544463] 4665 total pagecache pages [ 122.549902] 139264 pages of RAM [ 122.549905] 3367 reserved pages [ 122.551925] 4665 total pagecache pages [ 122.557679] 139264 pages of RAM [ 122.557682] 3367 reserved pages [ 122.561911] 4665 total pagecache pages [ 122.567090] 139264 pages of RAM [ 122.567092] 3367 reserved pages [ 122.571902] 4665 total pagecache pages [ 122.576763] 139264 pages of RAM [ 122.576765] 3367 reserved pages [ 122.576767] 2235 slab pages [ 122.576769] 263437 pages shared [ 122.576770] 0 pages swap cached [ 122.581730] syslog-ng: page allocation failure: order:0, mode:0x201db [ 122.581734] CPU: 0 PID: 2046 Comm: syslog-ng Tainted: G O 3.10.72-gca334de #1 [ 122.581747] [<c00159c0>] (unwind_backtrace+0x0/0xf8) from [<c0011abc>] (show_stack+0x10/0x14) [ 122.581756] [<c0011abc>] (show_stack+0x10/0x14) from [<c009db40>] (warn_alloc_failed+0xa8/0x120) [ 122.581765] [<c009db40>] (warn_alloc_failed+0xa8/0x120) from [<c00a0a60>] (__alloc_pages_nodemask+0x614/0x8c8) [ 122.581772] [<c00a0a60>] (__alloc_pages_nodemask+0x614/0x8c8) from [<c009b7b0>] (filemap_fault+0x1c8/0x410) [ 122.581779] [<c009b7b0>] (filemap_fault+0x1c8/0x410) from [<c00b7340>] (__do_fault+0x68/0x560) [ 122.581786] [<c00b7340>] (__do_fault+0x68/0x560) from [<c00b9a1c>] (handle_pte_fault+0x90/0x1164) [ 122.581792] [<c00b9a1c>] (handle_pte_fault+0x90/0x1164) from [<c00bbb60>] (handle_mm_fault+0xec/0x154) [ 122.581801] [<c00bbb60>] (handle_mm_fault+0xec/0x154) from [<c050e134>] (do_page_fault.part.7+0x1d8/0x36c) [ 122.581809] [<c050e134>] (do_page_fault.part.7+0x1d8/0x36c) from [<c050e328>] (do_page_fault+0x60/0x6c) [ 122.581816] [<c050e328>] (do_page_fault+0x60/0x6c) from [<c0008490>] (do_PrefetchAbort+0x2c/0x94) [ 122.581822] [<c0008490>] (do_PrefetchAbort+0x2c/0x94) from [<c050cdd4>] (ret_from_exception+0x0/0x10) [ 122.581824] Exception stack(0xdd65dfb0 to 0xdd65dff8) [ 122.581828] dfa0: 00000001 bed63b98 00000008 0010efc8 [ 122.581833] dfc0: bed63b98 00000455 bed63c48 000000fc bed63c20 00013800 000003e8 bed63c44 [ 122.581837] dfe0: 00000000 bed63b94 b6eedbdc b6cd054c 600f0010 ffffffff [ 122.581838] Mem-info: [ 122.581841] DMA per-cpu: [ 122.581844] CPU 0: hi: 186, btch: 31 usd: 39 [ 122.581847] CPU 1: hi: 186, btch: 31 usd: 153 [ 122.581849] CPU 2: hi: 186, btch: 31 usd: 177 [ 122.581852] CPU 3: hi: 186, btch: 31 usd: 65 [ 122.581860] active_anon:123198 inactive_anon:3876 isolated_anon:0 [ 122.581860] active_file:25 inactive_file:9 isolated_file:32 [ 122.581860] unevictable:0 dirty:0 writeback:0 unstable:0 [ 122.581860] free:703 slab_reclaimable:902 slab_unreclaimable:2876 [ 122.581860] mapped:48 shmem:4573 pagetables:787 bounce:0 [ 122.581860] free_cma:9 [ 122.581870] DMA free:2812kB min:2900kB low:3624kB high:4348kB active_anon:492792kB inactive_anon:15504kB active_file:100kB inactive_file:36kB unevictable:0kB isolated(anon):0kB isolated(file):128kB prs [ 122.581877] lowmem_reserve[]: 0 0 0 0 [ 122.581899] DMA: 1*4kB (R) 0*8kB 0*16kB 1*32kB (R) 0*64kB 0*128kB 1*256kB (R) 1*512kB (R) 0*1024kB 1*2048kB (R) 0*4096kB = 2852kB [ 122.581900] 4665 total pagecache pages [ 122.586573] 139264 pages of RAM [ 122.586574] 1473 free pages [ 122.586575] 3367 reserved pages [ 122.586577] 2235 slab pages [ 122.586579] 263437 pages shared [ 122.586580] 0 pages swap cached [ 122.591718] syslog-ng: page allocation failure: order:0, mode:0x201db [ 122.591723] CPU: 0 PID: 2046 Comm: syslog-ng Tainted: G O 3.10.72-gca334de #1 [ 122.591736] [<c00159c0>] (unwind_backtrace+0x0/0xf8) from [<c0011abc>] (show_stack+0x10/0x14) [ 122.591746] [<c0011abc>] (show_stack+0x10/0x14) from [<c009db40>] (warn_alloc_failed+0xa8/0x120) [ 122.591754] [<c009db40>] (warn_alloc_failed+0xa8/0x120) from [<c00a0a60>] (__alloc_pages_nodemask+0x614/0x8c8) [ 122.591761] [<c00a0a60>] (__alloc_pages_nodemask+0x614/0x8c8) from [<c009b7b0>] (filemap_fault+0x1c8/0x410) [ 122.591768] [<c009b7b0>] (filemap_fault+0x1c8/0x410) from [<c00b7340>] (__do_fault+0x68/0x560) [ 122.591775] [<c00b7340>] (__do_fault+0x68/0x560) from [<c00b9a1c>] (handle_pte_fault+0x90/0x1164) [ 122.591781] [<c00b9a1c>] (handle_pte_fault+0x90/0x1164) from [<c00bbb60>] (handle_mm_fault+0xec/0x154) [ 122.591789] [<c00bbb60>] (handle_mm_fault+0xec/0x154) from [<c050e134>] (do_page_fault.part.7+0x1d8/0x36c) [ 122.591797] [<c050e134>] (do_page_fault.part.7+0x1d8/0x36c) from [<c050e328>] (do_page_fault+0x60/0x6c) [ 122.591804] [<c050e328>] (do_page_fault+0x60/0x6c) from [<c0008490>] (do_PrefetchAbort+0x2c/0x94) [ 122.591810] [<c0008490>] (do_PrefetchAbort+0x2c/0x94) from [<c050cdd4>] (ret_from_exception+0x0/0x10) [ 122.591812] Exception stack(0xdd65dfb0 to 0xdd65dff8) [ 122.591816] dfa0: 00000001 bed63b98 00000008 0010efc8 [ 122.591821] dfc0: bed63b98 00000455 bed63c48 000000fc bed63c20 00013800 000003e8 bed63c44 [ 122.591824] dfe0: 00000000 bed63b94 b6eedbdc b6cd054c 600f0010 ffffffff [ 122.591826] Mem-info: [ 122.591828] DMA per-cpu: [ 122.591831] CPU 0: hi: 186, btch: 31 usd: 39 [ 122.591833] CPU 1: hi: 186, btch: 31 usd: 153 [ 122.591836] CPU 2: hi: 186, btch: 31 usd: 177 [ 122.591838] CPU 3: hi: 186, btch: 31 usd: 65 [ 122.591846] active_anon:123198 inactive_anon:3876 isolated_anon:0 [ 122.591846] active_file:25 inactive_file:9 isolated_file:32 [ 122.591846] unevictable:0 dirty:0 writeback:0 unstable:0 [ 122.591846] free:703 slab_reclaimable:902 slab_unreclaimable:2876 [ 122.591846] mapped:48 shmem:4573 pagetables:787 bounce:0 [ 122.591846] free_cma:9 [ 122.591857] DMA free:2812kB min:2900kB low:3624kB high:4348kB active_anon:492792kB inactive_anon:15504kB active_file:100kB inactive_file:36kB unevictable:0kB isolated(anon):0kB isolated(file):128kB prs [ 122.591864] lowmem_reserve[]: 0 0 0 0 [ 122.591887] DMA: 1*4kB (R) 0*8kB 0*16kB 1*32kB (R) 0*64kB 0*128kB 1*256kB (R) 1*512kB (R) 0*1024kB 1*2048kB (R) 0*4096kB = 2852kB [ 122.591889] 4665 total pagecache pages [ 122.596425] 139264 pages of RAM [ 122.596427] 1473 free pages [ 122.596428] 3367 reserved pages [ 122.596430] 2235 slab pages [ 122.596431] 263437 pages shared [ 122.596433] 0 pages swap cached [ 122.601709] syslog-ng: page allocation failure: order:0, mode:0x201db [ 122.601714] CPU: 0 PID: 2046 Comm: syslog-ng Tainted: G O 3.10.72-gca334de #1 [ 122.601728] [<c00159c0>] (unwind_backtrace+0x0/0xf8) from [<c0011abc>] (show_stack+0x10/0x14) [ 122.601738] [<c0011abc>] (show_stack+0x10/0x14) from [<c009db40>] (warn_alloc_failed+0xa8/0x120) [ 122.601748] [<c009db40>] (warn_alloc_failed+0xa8/0x120) from [<c00a0a60>] (__alloc_pages_nodemask+0x614/0x8c8) [ 122.601755] [<c00a0a60>] (__alloc_pages_nodemask+0x614/0x8c8) from [<c009b7b0>] (filemap_fault+0x1c8/0x410) [ 122.601763] [<c009b7b0>] (filemap_fault+0x1c8/0x410) from [<c00b7340>] (__do_fault+0x68/0x560) [ 122.601769] [<c00b7340>] (__do_fault+0x68/0x560) from [<c00b9a1c>] (handle_pte_fault+0x90/0x1164) [ 122.601776] [<c00b9a1c>] (handle_pte_fault+0x90/0x1164) from [<c00bbb60>] (handle_mm_fault+0xec/0x154) [ 122.601784] [<c00bbb60>] (handle_mm_fault+0xec/0x154) from [<c050e134>] (do_page_fault.part.7+0x1d8/0x36c) [ 122.601792] [<c050e134>] (do_page_fault.part.7+0x1d8/0x36c) from [<c050e328>] (do_page_fault+0x60/0x6c) [ 122.601799] [<c050e328>] (do_page_fault+0x60/0x6c) from [<c0008490>] (do_PrefetchAbort+0x2c/0x94) [ 122.601805] [<c0008490>] (do_PrefetchAbort+0x2c/0x94) from [<c050cdd4>] (ret_from_exception+0x0/0x10) [ 122.601808] Exception stack(0xdd65dfb0 to 0xdd65dff8) [ 122.601812] dfa0: 00000001 bed63b98 00000008 0010efc8 [ 122.601816] dfc0: bed63b98 00000455 bed63c48 000000fc bed63c20 00013800 000003e8 bed63c44 [ 122.601820] dfe0: 00000000 bed63b94 b6eedbdc b6cd054c 600f0010 ffffffff [ 122.601822] Mem-info: [ 122.601823] DMA per-cpu: [ 122.601826] CPU 0: hi: 186, btch: 31 usd: 39 [ 122.601828] CPU 1: hi: 186, btch: 31 usd: 153 [ 122.601831] CPU 2: hi: 186, btch: 31 usd: 177 [ 122.601834] CPU 3: hi: 186, btch: 31 usd: 65 [ 122.601842] active_anon:123198 inactive_anon:3876 isolated_anon:0 [ 122.601842] active_file:25 inactive_file:9 isolated_file:32 [ 122.601842] unevictable:0 dirty:0 writeback:0 unstable:0 [ 122.601842] free:703 slab_reclaimable:902 slab_unreclaimable:2876 [ 122.601842] mapped:48 shmem:4573 pagetables:787 bounce:0 [ 122.601842] free_cma:9 [ 122.601854] DMA free:2812kB min:2900kB low:3624kB high:4348kB active_anon:492792kB inactive_anon:15504kB active_file:100kB inactive_file:36kB unevictable:0kB isolated(anon):0kB isolated(file):128kB prs [ 122.601860] lowmem_reserve[]: 0 0 0 0 [ 122.601883] DMA: 1*4kB (R) 0*8kB 0*16kB 1*32kB (R) 0*64kB 0*128kB 1*256kB (R) 1*512kB (R) 0*1024kB 1*2048kB (R) 0*4096kB = 2852kB [ 122.601884] 4665 total pagecache pages [ 122.606313] 139264 pages of RAM [ 122.606314] 1473 free pages [ 122.606316] 3367 reserved pages [ 122.606317] 2235 slab pages [ 122.606318] 263437 pages shared [ 122.606320] 0 pages swap cached [ 122.611713] syslog-ng: page allocation failure: order:0, mode:0x201db [ 122.611717] CPU: 0 PID: 2046 Comm: syslog-ng Tainted: G O 3.10.72-gca334de #1 [ 122.611730] [<c00159c0>] (unwind_backtrace+0x0/0xf8) from [<c0011abc>] (show_stack+0x10/0x14) [ 122.611740] [<c0011abc>] (show_stack+0x10/0x14) from [<c009db40>] (warn_alloc_failed+0xa8/0x120) [ 122.611748] [<c009db40>] (warn_alloc_failed+0xa8/0x120) from [<c00a0a60>] (__alloc_pages_nodemask+0x614/0x8c8) [ 122.611755] [<c00a0a60>] (__alloc_pages_nodemask+0x614/0x8c8) from [<c009b7b0>] (filemap_fault+0x1c8/0x410) [ 122.611761] [<c009b7b0>] (filemap_fault+0x1c8/0x410) from [<c00b7340>] (__do_fault+0x68/0x560) [ 122.611768] [<c00b7340>] (__do_fault+0x68/0x560) from [<c00b9a1c>] (handle_pte_fault+0x90/0x1164) [ 122.611774] [<c00b9a1c>] (handle_pte_fault+0x90/0x1164) from [<c00bbb60>] (handle_mm_fault+0xec/0x154) [ 122.611782] [<c00bbb60>] (handle_mm_fault+0xec/0x154) from [<c050e134>] (do_page_fault.part.7+0x1d8/0x36c) [ 122.611790] [<c050e134>] (do_page_fault.part.7+0x1d8/0x36c) from [<c050e328>] (do_page_fault+0x60/0x6c) [ 122.611797] [<c050e328>] (do_page_fault+0x60/0x6c) from [<c0008490>] (do_PrefetchAbort+0x2c/0x94) [ 122.611803] [<c0008490>] (do_PrefetchAbort+0x2c/0x94) from [<c050cdd4>] (ret_from_exception+0x0/0x10) [ 122.611806] Exception stack(0xdd65dfb0 to 0xdd65dff8) [ 122.611809] dfa0: 00000001 bed63b98 00000008 0010efc8 [ 122.611814] dfc0: bed63b98 00000455 bed63c48 000000fc bed63c20 00013800 000003e8 bed63c44 [ 122.611818] dfe0: 00000000 bed63b94 b6eedbdc b6cd054c 600f0010 ffffffff [ 122.611820] Mem-info: [ 122.611821] DMA per-cpu: [ 122.611824] CPU 0: hi: 186, btch: 31 usd: 39 [ 122.611827] CPU 1: hi: 186, btch: 31 usd: 153 [ 122.611829] CPU 2: hi: 186, btch: 31 usd: 177 [ 122.611831] CPU 3: hi: 186, btch: 31 usd: 65 [ 122.611840] active_anon:123198 inactive_anon:3876 isolated_anon:0 [ 122.611840] active_file:25 inactive_file:9 isolated_file:32 [ 122.611840] unevictable:0 dirty:0 writeback:0 unstable:0 [ 122.611840] free:703 slab_reclaimable:902 slab_unreclaimable:2876 [ 122.611840] mapped:48 shmem:4573 pagetables:787 bounce:0 [ 122.611840] free_cma:9 [ 122.611850] DMA free:2812kB min:2900kB low:3624kB high:4348kB active_anon:492792kB inactive_anon:15504kB active_file:100kB inactive_file:36kB unevictable:0kB isolated(anon):0kB isolated(file):128kB prs [ 122.611857] lowmem_reserve[]: 0 0 0 0 [ 122.611879] DMA: 1*4kB (R) 0*8kB 0*16kB 1*32kB (R) 0*64kB 0*128kB 1*256kB (R) 1*512kB (R) 0*1024kB 1*2048kB (R) 0*4096kB = 2852kB [ 122.611881] 4665 total pagecache pages [ 122.616280] 139264 pages of RAM [ 122.616281] 1473 free pages [ 122.616282] 3367 reserved pages [ 122.616284] 2235 slab pages [ 122.616285] 263437 pages shared [ 122.616288] 0 pages swap cached [ 122.621731] syslog-ng: page allocation failure: order:0, mode:0x201db [ 122.621736] CPU: 0 PID: 2046 Comm: syslog-ng Tainted: G O 3.10.72-gca334de #1 [ 122.621750] [<c00159c0>] (unwind_backtrace+0x0/0xf8) from [<c0011abc>] (show_stack+0x10/0x14) [ 122.621759] [<c0011abc>] (show_stack+0x10/0x14) from [<c009db40>] (warn_alloc_failed+0xa8/0x120) [ 122.621767] [<c009db40>] (warn_alloc_failed+0xa8/0x120) from [<c00a0a60>] (__alloc_pages_nodemask+0x614/0x8c8) [ 122.621774] [<c00a0a60>] (__alloc_pages_nodemask+0x614/0x8c8) from [<c009b7b0>] (filemap_fault+0x1c8/0x410) [ 122.621781] [<c009b7b0>] (filemap_fault+0x1c8/0x410) from [<c00b7340>] (__do_fault+0x68/0x560) [ 122.621787] [<c00b7340>] (__do_fault+0x68/0x560) from [<c00b9a1c>] (handle_pte_fault+0x90/0x1164) [ 122.621794] [<c00b9a1c>] (handle_pte_fault+0x90/0x1164) from [<c00bbb60>] (handle_mm_fault+0xec/0x154) [ 122.621803] [<c00bbb60>] (handle_mm_fault+0xec/0x154) from [<c050e134>] (do_page_fault.part.7+0x1d8/0x36c) [ 122.621812] [<c050e134>] (do_page_fault.part.7+0x1d8/0x36c) from [<c050e328>] (do_page_fault+0x60/0x6c) [ 122.621818] [<c050e328>] (do_page_fault+0x60/0x6c) from [<c0008490>] (do_PrefetchAbort+0x2c/0x94) [ 122.621825] [<c0008490>] (do_PrefetchAbort+0x2c/0x94) from [<c050cdd4>] (ret_from_exception+0x0/0x10) [ 122.621828] Exception stack(0xdd65dfb0 to 0xdd65dff8) [ 122.621832] dfa0: 00000001 bed63b98 00000008 0010efc8 [ 122.621836] dfc0: bed63b98 00000455 bed63c48 000000fc bed63c20 00013800 000003e8 bed63c44 [ 122.621840] dfe0: 00000000 bed63b94 b6eedbdc b6cd054c 600f0010 ffffffff [ 122.621842] Mem-info: [ 122.621843] DMA per-cpu: [ 122.621846] CPU 0: hi: 186, btch: 31 usd: 39 [ 122.621849] CPU 1: hi: 186, btch: 31 usd: 153 [ 122.621851] CPU 2: hi: 186, btch: 31 usd: 177 [ 122.621853] CPU 3: hi: 186, btch: 31 usd: 65 [ 122.621861] active_anon:123198 inactive_anon:3876 isolated_anon:0 [ 122.621861] active_file:25 inactive_file:9 isolated_file:32 [ 122.621861] unevictable:0 dirty:0 writeback:0 unstable:0 [ 122.621861] free:703 slab_reclaimable:902 slab_unreclaimable:2876 [ 122.621861] mapped:48 shmem:4573 pagetables:787 bounce:0 [ 122.621861] free_cma:9 [ 122.621872] DMA free:2812kB min:2900kB low:3624kB high:4348kB active_anon:492792kB inactive_anon:15504kB active_file:100kB inactive_file:36kB unevictable:0kB isolated(anon):0kB isolated(file):128kB prs [ 122.621879] lowmem_reserve[]: 0 0 0 0 [ 122.621901] DMA: 1*4kB (R) 0*8kB 0*16kB 1*32kB (R) 0*64kB 0*128kB 1*256kB (R) 1*512kB (R) 0*1024kB 1*2048kB (R) 0*4096kB = 2852kB [ 122.621902] 4665 total pagecache pages [ 122.626290] 139264 pages of RAM [ 122.626291] 1473 free pages [ 122.626292] 3367 reserved pages [ 122.626294] 2235 slab pages [ 122.626295] 263437 pages shared [ 122.626296] 0 pages swap cached [ 124.022116] [<c05076a0>] (dump_header.isra.14+0x78/0x198) from [<c009c8a0>] (oom_kill_process+0x368/0x3dc) [ 124.031742] [<c009c8a0>] (oom_kill_process+0x368/0x3dc) from [<c009cdb0>] (out_of_memory+0x2a4/0x2f8) [ 124.040936] [<c009cdb0>] (out_of_memory+0x2a4/0x2f8) from [<c00a0ce8>] (__alloc_pages_nodemask+0x89c/0x8c8) [ 124.050650] [<c00a0ce8>] (__alloc_pages_nodemask+0x89c/0x8c8) from [<c00ba440>] (handle_pte_fault+0xab4/0x1164) [ 124.060709] [<c00ba440>] (handle_pte_fault+0xab4/0x1164) from [<c00bbb60>] (handle_mm_fault+0xec/0x154) [ 124.070069] [<c00bbb60>] (handle_mm_fault+0xec/0x154) from [<c050e134>] (do_page_fault.part.7+0x1d8/0x36c) [ 124.079694] [<c050e134>] (do_page_fault.part.7+0x1d8/0x36c) from [<c050e328>] (do_page_fault+0x60/0x6c) [ 124.089059] [<c050e328>] (do_page_fault+0x60/0x6c) from [<c00083fc>] (do_DataAbort+0x2c/0x94) [ 124.097561] [<c00083fc>] (do_DataAbort+0x2c/0x94) from [<c050cb74>] (__dabt_usr+0x34/0x40) [ 124.105796] Exception stack(0xdf9edfb0 to 0xdf9edff8) [ 124.110838] dfa0: 00002021 0001c179 380a1e88 00000000 [ 124.118980] dfc0: 00000000 b6e344c8 b6e344f8 3809fe70 000001ff 0001e198 0003d368 b6e34500 [ 124.127131] dfe0: b6e344c8 bed32640 b6dab351 b6da952e 00000030 ffffffff [ 124.133727] Mem-info: [ 124.135986] DMA per-cpu: [ 124.138507] CPU 0: hi: 186, btch: 31 usd: 39 [ 124.143280] CPU 1: hi: 186, btch: 31 usd: 153 [ 124.148046] CPU 2: hi: 186, btch: 31 usd: 177 [ 124.152817] CPU 3: hi: 186, btch: 31 usd: 65 [ 124.157589] active_anon:123209 inactive_anon:3876 isolated_anon:0 [ 124.157589] active_file:19 inactive_file:11 isolated_file:32 [ 124.157589] unevictable:0 dirty:0 writeback:0 unstable:0 [ 124.157589] free:721 slab_reclaimable:902 slab_unreclaimable:2876 [ 124.157589] mapped:59 shmem:4573 pagetables:795 bounce:0 [ 124.157589] free_cma:0 [ 124.188662] DMA free:2884kB min:2900kB low:3624kB high:4348kB active_anon:492836kB inactive_anon:15504kB active_file:76kB inactive_file:44kB unevictable:0kB isolated(anon):0kB isolated(file):128kB preo [ 124.230269] lowmem_reserve[]: 0 0 0 0 [ 124.233949] DMA: 1*4kB (R) 0*8kB 0*16kB 2*32kB (UR) 0*64kB 0*128kB 1*256kB (R) 1*512kB (R) 0*1024kB 1*2048kB (R) 0*4096kB = 2884kB [ 124.245757] 4608 total pagecache pages [ 124.254280] 139264 pages of RAM [ 124.257403] 1531 free pages [ 124.260176] 3367 reserved pages [ 124.263304] 2235 slab pages [ 124.266078] 263245 pages shared [ 124.269198] 0 pages swap cached [ 124.272328] [ pid ] uid tgid total_vm rss nr_ptes swapents oom_score_adj name [ 124.280194] [ 1347] 0 1347 661 102 4 0 -1000 udevd [ 124.288085] [ 1961] 997 1961 588 38 4 0 0 dbus-daemon [ 124.296494] [ 1983] 0 1983 35826 62 69 0 0 mpmsrv [ 124.304471] [ 1999] 0 1999 472 41 4 0 0 rmServer.out [ 124.312965] [ 2003] 0 2003 467 16 3 0 0 telnetd [ 124.321027] [ 2006] 0 2006 376 22 3 0 0 lad_tci6638 [ 124.329425] [ 2013] 0 2013 660 104 4 0 -1000 udevd [ 124.337312] [ 2014] 0 2014 660 104 4 0 -1000 udevd [ 124.345200] [ 2018] 999 2018 483 48 4 0 0 rpcbind [ 124.353265] [ 2031] 998 2031 419 34 3 0 0 rpc.statd [ 124.361500] [ 2037] 0 2037 536 29 4 0 0 dropbear [ 124.369641] [ 2045] 0 2045 863 42 4 0 0 syslog-ng [ 124.377873] [ 2046] 0 2046 1591 219 6 0 0 syslog-ng [ 124.386105] [ 2182] 0 2182 657 63 4 0 0 login [ 124.393991] [ 2183] 0 2183 652 59 4 0 0 sh [ 124.401619] [ 2184] 0 2184 652 82 4 0 0 bash [ 124.409414] [ 2189] 0 2189 230529 121206 452 0 0 mpirun [ 124.417388] [ 2190] 0 2190 681 46 3 0 0 ssh [ 124.425106] [ 2191] 0 2191 105251 299 209 0 0 nbody [ 124.432993] Out of memory: Kill process 2189 (mpirun) score 868 or sacrifice child [ 124.440535] Killed process 2191 (nbody) total-vm:421004kB, anon-rss:1196kB, file-rss:0kB -------------------------------------------------------------------------- mpirun noticed that process rank 0 with PID 2191 on node DSP1 exited on signal 9 (Killed). -------------------------------------------------------------------------- INK send EDMA_TRANSFER (to a2800000 from a2000000, size=28160! 00000, size=28160! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)! [DSP1:02191] BTL_HLINK no room in FIFO (send)!
I was looking for the source code of the ti-openmpi module but I did not found it with verison control. Only found this:
But I don't know how this is related to ti-openmpi in mcsdk-hpc package.
Please provide ti-openmpi source code. Please provide help to solve this issue with ti-openmpi. We have a very big project, which uses ti-openmpi over hyperlink prototyped on evaluation modules. We need it to work on custom hardware too. The hyperlink seems functioning properly. Do you have any idea about this FIFO full issue in the nbody log? What causes these strange kernel errors in the trace? Can this issue be related with, that the DSP0 hyperlink-0 port is connected with DSP1 hyperlink-1 port ? I think this should be transparent.I am using mcsdk-3_01_04_07. This is the latest version of mcsdk. We could not migrate to processor SDK, because Hyperlink and openmpi not supported on that. Please provide support to us.
Thanks for Your help.
Dávid Huber