This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

### DM6446 Nand Boot

Hello


I seem to have an issue booting from NAND flash.

IT seems like the DM6446 pulls the UBL from NAND, but it does not execute
it, it just keeps saying BOOTME

If we force the UBL to be downloaded via UART, then it executes, identifies
the NAND, pulls U-BOOT/kernel/nfs/etc/etc and runs just fine.

 

We are using the newer DM6446 part # TMS320DM6446AZWTA

I think this also now supports a SPI FLASH boot?
Is there a new MAGIC ID code or something that needs to be put into NAND for
the UBL?


We are using DVFLasher (I know it's a bit old, but it has been solid for us)

 

If anyone can provide some thoughts -that would be great

 

Thanks