As DDR3 device usually EOL, customer needs to prepare backup stock of DDR3 device. but different DDR3 device got different writing leveling result.
So customer asks:
#1. If only use signal 16bit DDR3 device, doesn't it need to do software leveling?
#2. What is mean of below parameters, what is the relation between those parameter to DDR timing? if there are small different between different DDR3 vendor, can they use the same set of parameter?
#define DATA_PHY_RD_DQS_SLAVE_RATIO 0x3A #define DATA_PHY_FIFO_WE_SLAVE_RATIO 0x11B //RD DQS GATE #define DATA_PHY_WR_DQS_SLAVE_RATIO 0xA8 #define DATA_PHY_WR_DATA_SLAVE_RATIO 0xE1 //WRITE DATA