This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5718: McASP module driver

Part Number: AM5718
Other Parts Discussed in Thread: SYSBIOS, TLV320AIC3106

Hi 

I have a custom board based am5718 with tlv320aic as audio device(i2c1 is used as interface for configuration)

I have ported alsa driver and verified the output. Since our design is an SDR Platform,it is necessary to change waveform when the linux is running.Some waveform access audio from linux (ARM) and some waveform from DSP(SYSBIOS).I have following queries

1)Is it possible to access McASP3 from DSP(since McASP3 and EDMA are used by linux)?

If possible,How it is possible?

If I convert McASP and EDMA as module driver,can my requirement be met

Regards

Satheesh Kumar S