Other Parts Discussed in Thread: TDA2
Hi~
There was a 0.3 version of the EMIF tool, so I tested ddr4 on uboot.
Do you have avator EMIF TOOL in tda4? And ask if you can provide it later.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TDA2
Hi~
Hi Kyungtae,
The TDA2x Avatar_EMIF_Tool did contain a CCS project that swept DLL values to optimize settings and account for system level timing skews.
Similarly, the TDA4M has hardware algorithms inside the PHY which perform a similar function to optimize DLL values based on skews introduced in the system, such as the PCB routing. By using the hardware algorithms, this simplifies the procedure to quickly bring up new boards, and also allows each system to have unique settings and compensate for any board-to-board skew differences.
The XLS tool Kyle has referenced already has the hardware training support enabled during initialization. Thus, the parameters are being optimized each boot cycle on TDA4M. Additional details regarding which parameters are trained can be found in section 8.2.4.7.9 (Memory Controllers -> DDR Subsystem -> DDRSS Functional Description -> DDR PHY Functional Description -> Training Support) of the TRM.
Since hardware algorithms are used on TDA4M, the use of software (such as the Avatar EMIF Tools) is not required or supported.
Best regards,
Kevin
Hi, Kevin.