Hi,
I have CCS 9.2 installed with Emu pack/patch version 8.3.1.00007 and 6.1.0 SDK.
I created a Target Configuration to be used when the A72 is running with Linux, as described in the docs.
Then when I wanted to connect to the C71 DSP it told me that the XDS firmware is out of date and I must update.
So I click yes and wait, then a message comes from CCS that it cannot connect, I shall power cycle my target, so I do that.
After that I still cannot connect, I get his:
Error connecting to the target:
(Error -261 @ 0x0)
Invalid response was received from the XDS110.
(Emulation package 8.3.1.00007)
I can see a USB device with the ID 0451:bef3. I xan update the FW via xdsdfu too and read the device ID.
But for some reason I cannot connect any more.