Hi All;
I am new to OMAP and CCS and I'm having some trouble configuring these two items to work together. We will not run Linux on the omap rather an embedded RTOS called Unision 5 and I need to setup CCS with the emulator.
I did the following:
- install ccs
- install emulator (blackhawk xds100v2 with 20 pin micro connector)
- install on logicpd board using their daughter card for emulators (EMT) and plugged in xds100v2 after removing the bigger 20 pin adapter using the microconnector with keying
- started ccs
- wrote trivial program and built it, generating all necessary output
- setup a general debug config with omap 3530 and tried it
- ccs crashed due to a jvm crash but did report a memory map problem at 0x00000000 before crashing
Suggestions? ideas?
Kim