Part Number: AM3352
Hi I have meet one usb babble issue during pppd link (when the system is up, we can see gsm modem is attached to ttyUSB0/1/2/3)
AM3352 usb as host, and EC25-AU is as slave, and they are wiring directly, and it had about 1% failure ratio
see below log:
pon 4G watting...
15[ 53.617591] musb-hdrc musb-hdrc.1: Babble
[ 53.621768] musb-hdrc musb-hdrc.1: Babble
[ 53.626067] usb 2-1: USB disconnect, device number 2
[ 53.645244] option1 ttyUSB0: GSM modem (1-port) converter now disconnected from ttyUSB0
[ 53.677880] option 2-1:1.0: device disconnected
[ 53.705286] option1 ttyUSB1: GSM modem (1-port) converter now disconnected from ttyUSB1
[ 53.744425] option 2-1:1.1: device disconnected
[ 53.768903] option1 ttyUSB2: GSM modem (1-port) converter now disconnected from ttyUSB2
[ 53.785435] option 2-1:1.2: device disconnected
[ 53.831944] option1 ttyUSB3: GSM modem (1-port) converter now disconnected from ttyUSB3
[ 53.869923] option 2-1:1.3: device disconnected