Other Parts Discussed in Thread: AM1707
In our project, we want to boot from NOR flash, but the hardware is not ready. so we test it on the AM1707 EVM,
we finished sft_AM1707_NOR, and use it flash the ubl_spi.bin to NOR flash. (we use ubl_spi because ubl_nor.bin has not finished.)
and write 0x000000F0 to 0x60000000 as configuration word.
I think the boot sequence should like this:
1. RBL read ubl_spi.bin to 0x80000000 and run it
2. ubl_spi.bin will copy uboot (reside in SPI flash) to RAM and run it
3.uboot boot linux
but when i power on the EVM , nothing happened, and the uart terminal display nothing.
I have set the bootmode and BOOT_DEVICE switch on the right position.
can anybody give me some advice?
English is not my native language, hope you can understand what i say.
thank you!