Part Number: TMS320C5545
Other Parts Discussed in Thread: OMAPL138
Since the C5545 is last-time-buy...what's the next logical place to move to from the C5545 BoosterPack?
I need a low-cost, fast DSP with FFT accelerator and a BLE radio on it, and the BoosterPack seems ideal (not sure if I'm going to use it with the actual LaunchPad or not)...
Also... are there peripheral examples (I'm used to the STMicro ecosystem) so that I can see how to program/use the I2S, I2C, FFT, etc, or am I going to have to hope I can get all the examples I need from the out-of-the-box source code?