This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP with external hardware ?



hi,

" TI’s OMAP™ platform provides a superior solution for the development
of speech applications on personal handheld devices."

With reference to above note,  OMAP1510 and OMAP5910 will provide speaker independent recognition for handheld device.

Just consider the instance of external hardware seems to be the robotic hand !!!

so whether is it possible to interconnect the OMAP 1510 or OMAP 5910  with ROBOTIC HAND,

so that as per speaker command, THE ROBOT HAND should recognize the speaker by means of OMAP 1510 or 5910 and THE ROBOT HAND should perform the action.

 

IS IT POSSIBLE?

eagerly waiting for ur reply