Part Number: AM3358
Dear sir,
here i used this sdk "ti-processor-sdk-linux-am335x-evm-06.01.00.08" and i build all
MLO
u-boot.img
-----------------
zImage
am335x-boneblack.dtb
------------------------
and Modules installed rootfs
--------------------------------------------------
for custom SD-card : by using "create-sdcard.sh", i have created boot & rootfs partitions and copied above files properly.
after that inserted in to BBB board here it's working fine and i got login prompt : root@am335x-evm#.
when i remove my sd card and i checked again my kernel version it's not my custom kernel it's showing previous version.
so, now i want to let these all should be flash on-board eMMC. please tell me the procedure and
Thanks
hari