Part Number: 66AK2G12
Hi,
I am designing a board with 66AK2G12 and I am using Clock tree tool v.1.0.0.2 that allow to select this device and silicon revision 1.0.
For my purpose I need to obtain a 25 MHz clock signal on CLKOUT ball H23 for two Ethernet phy in MII mode. According to SPRUHY8I TRM, I can use NSS/IEP PLL that generates 1GHz clock signal, divided for 20 factor, obtain 50MHz. Through a 2 factor of division and the mux enable signal set to 1, I obtain 25 Mhz at the output.
Now I am checking with CTT if this choice is correct but I see that the division factor is 200 and not 20, 2.5 MHz clock signal reaches the CLKOUT pad and not 25 MHz.
Please can you confirm that this is an error on CTT and the TRM is correct?
Regards
Graziano Rufolo
Hardware/Firmware Engineer
Hitachi Rail