This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't install xdctools, cgt or bios on Linux

I bought a BeagleBoard a couple of weeks ago and I'm still in the process of setting up a build environment for it.  I'm using OpenEmbedded and it requires that certain packages be installed manually due to licensing restrictions.  I've followed the instructions in OpenEmbedded (and from a bunch of other web sites), but I simply can't get these packages to install.

Specifically, I have downloaded bios_setuplinux_5_41_09_34.bin, xdctools_setuplinux_3_20_06_81.bin and ti_cgt_c6000_6.1.18_setup_linux_x86.bin from TI's web site onto my Linux system (Fedora 14).  I've done a chmod +x on all the files, but when I try to run them, they immediately exit with a return code of 127.  They're statically linked, so I don't think I have any dependency issues.

Does anyone know what I'm doing wrong?