Hello,
while building sdk for TDA4 encountering some errors and errors are mentioned below
ERROR: external-arm-toolchain-2019.03-r0 do_install: Function failed: do_install (log file is located at /home/che7-l20149/TDA4/SDK/yocto-build/build/arago-tmp-external-arm-toolchain/work/aarch64-linux/external-arm-toolchain/2019.03-r0/temp/log.do_install.13534)
ERROR: Logfile of failure stored in: /home/che7-l20149/TDA4/SDK/yocto-build/build/arago-tmp-external-arm-toolchain/work/aarch64-linux/external-arm-toolchain/2019.03-r0/temp/log.do_install.13534
log.do_install.13534 contain
DEBUG: Executing python function extend_recipe_sysroot
NOTE: Direct dependencies are ['/home/che7-l20149/TDA4/SDK/yocto-build/sources/oe-core/meta/recipes-devtools/quilt/quilt-native_0.65.bb:do_populate_sysroot', 'virtual:native:/home/che7-l20149/TDA4/SDK/yocto-build/sources/oe-core/meta/recipes-extended/xz/xz_5.2.4.bb:do_populate_sysroot', 'virtual:native:/home/che7-l20149/TDA4/SDK/yocto-build/sources/oe-core/meta/recipes-devtools/pkgconfig/pkgconfig_git.bb:do_populate_sysroot', 'virtual:native:/home/che7-l20149/TDA4/SDK/yocto-build/sources/oe-core/meta/recipes-devtools/bison/bison_3.0.4.bb:do_populate_sysroot', 'virtual:native:/home/che7-l20149/TDA4/SDK/yocto-build/sources/oe-core/meta/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot']
NOTE: Installed into sysroot: []
NOTE: Skipping as already exists in sysroot: ['quilt-native', 'xz-native', 'pkgconfig-native', 'bison-native', 'pseudo-native', 'automake-native', 'gnu-config-native', 'flex-native', 'libtool-native', 'autoconf-native', 'gettext-minimal-native', 'texinfo-dummy-native', 'm4-native']
DEBUG: Python function extend_recipe_sysroot finished
DEBUG: Executing shell function do_install
cp: cannot stat '../../../Toolchains/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu/aarch64-linux-gnu/lib64/*': No such file or directory
WARNING: exit code 1 from a shell command.
ERROR: Function failed: do_install (log file is located at /home/che7-l20149/TDA4/SDK/yocto-build/build/arago-tmp-external-arm-toolchain/work/aarch64-linux/external-arm-toolchain/2019.03-r0/temp/log.do_install.13534)
can anyone say what could be the reason?
thanks,
Akshatha