This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NetworkRx to Isp (Image Processing Issue)

Hi

I am sending the bayer_raw image using network_tx.exe tool to a usecase for processing.

THe usecase structure is :

NetworkRx -> IssM2mIsp -> Display

IssM2mIsp -> Alg_aewb

I am able to send the image and i am seeing output over display but the image on the display is not expected one.

I have an Bayer_raw with grbg format (8 bit and 12 bit )  which will result into an green image  when i converted it into rgb888, but when i send the same image into the usecase it is producing a different colour.

I am using tda2px and vsdk3.0.3.

Please help me in processing the image correctly and also please mention the configuration which i have to setup to do this image processing.

Thanks and Regards,

Aneesh

  • can you please attach the input (12b bayer) and ISP output (8b NV12) images?

  • grbg_12b.raw.txt

    Hi Mayank,

    The Input Image is attached above .

    .raw extension is not allowed. So,please remove the .txt extension of the file.

    I don't have the output image,the output is over hdmi.

    Regards,

    Aneesh

     

  • Thanks.. RAW image looks OK.

    In the standard usecase (image sensor driven), Process function M2MISP Link is called every time a frame is received from the sensor. Sensor driver has linkages to DCC, which is a tuning library. All of this is needed to correctly process the RAW images and get correct ISP output.

    I am not sure what changes you have done to the SW, but if you do it correctly you should be able to save YUV images after ISP. Please refer to 1-ch ISP capture display usecase.

  • Hi Mayank,

    I did not found the difference when compared with the 1-ch ISP capture display usecase and  i did not understand your first statement clearly (specially "DCC"). Can you please elaborate that part.

    Regards,

    Aneesh

  • Hi Mayank,

    Can I contact you directly regarding this issue.

    Regards,

    Aneesh 

  • Aneesh,

    It is better to communicate through E2E. This allows for all the experts to watch this thread and contribute.

    DCC is Dynamic Camera Configuration. This is a database of all ISP parameters required to process a RAW image correctly. This needs to be developed fro every sensor. This would need to be done for Network source also.

    Regards,

    Mayank

  • #include "chains_network_isp_display_priv.h"
    #include <src/include/chains_common.h>
    #include <src/rtos/iss/include/app_util_iss.h>
    #include <src/rtos/iss/include/iss_sensors.h>
    #include <src/rtos/iss/include/iss_utils.h>
    #include "../hm_raw_option/hm_raw_option_settings.h"
    
    #define ALG_AEWB_MEM_SIZE (896 * 1024)
    
    #define NETWORK_RX_FRAME_WIDTH      (1820)
    #define NETWORK_RX_FRAME_HEIGHT     (940)
    
    Void ChainsCommon_SetNetworkRxPrms_ND(
                            NetworkRxLink_CreateParams *pPrm,
                            UInt32 maxWidth,
                            UInt32 maxHeight,
                            UInt32 numCh,
                            UInt32 fps /* in msecs */
                            );
    
    typedef struct
    {
    	chains_network_isp_displayObj ucObj;
    	UInt32 captureOutWidth;
    	UInt32 captureOutHeight;
    	UInt32 displayWidth;
    	UInt32 displayHeight;
    	Chains_Ctrl *chainsCfg;
    	AppUtils_Obj appSensInfo;
    	UInt32  netProcId;
    	char enable_network_raw_frames[8];
    }chains_network_isp_displayAppObj;
    
    char gchains_network_isp_display_runTimeMenu[]={
    			"\r\n "
    		    "\r\n ===================="
    		    "\r\n chains Run-time Menu"
    		    "\r\n ===================="
    		    "\r\n "
    		    "\r\n 0: Stop Chain"
    		    "\r\n p: Print Performance Statistics "
    		    "\r\n "
    		    "\r\n Enter Choice: "
    		    "\r\n "};
    
    void chains_network_isp_display_FreeMemory(chains_network_isp_displayAppObj *pObj)
    {
    	Int32 status;
    
    	    IssM2mIspLink_CreateParams *pIssM2mIspPrm;
    	    AlgorithmLink_IssAewbCreateParams *pAlg_IssAewbPrm;
    
    
    	    pIssM2mIspPrm = &pObj->ucObj.IssM2mIspPrm;
    	    pAlg_IssAewbPrm = &pObj->ucObj.Alg_IssAewbPrm;
    
    	    if (pAlg_IssAewbPrm->memAllocInfo.memAddr)
    	    {
    	        status = Utils_memFree(UTILS_HEAPID_DDR_CACHED_SR,
    	                               (Ptr) pAlg_IssAewbPrm->memAllocInfo.memAddr,
    	                               pAlg_IssAewbPrm->memAllocInfo.memSize);
    	        UTILS_assert(status == 0);
    	    }
    
    	    if (pIssM2mIspPrm->memAllocInfo.memAddr)
    	    {
    	        status = Utils_memFree(UTILS_HEAPID_DDR_CACHED_SR,
    	                               (Ptr) pIssM2mIspPrm->memAllocInfo.memAddr,
    	                               pIssM2mIspPrm->memAllocInfo.memSize);
    	        UTILS_assert(status == 0);
    	    }
    }
    Void chains_network_isp_display_SetDisplayPrms(DisplayLink_CreateParams *pPrm_Video,
                                           Chains_DisplayType displayType,
                                           UInt32 displayWidth,
                                           UInt32 displayHeight,
                                           UInt32 captureWidth,
                                           UInt32 captureHeight)
    {
        UInt32 dispWidth, dispHeight;
    
        if (pPrm_Video)
        {
            if ((displayType == CHAINS_DISPLAY_TYPE_SDTV_NTSC)
                    || (displayType == CHAINS_DISPLAY_TYPE_SDTV_PAL))
            {
                pPrm_Video->displayScanFormat = SYSTEM_SF_INTERLACED;
            }
    
            /* To maintain the aspect ratio, change the display tarWidth */
            dispWidth = captureWidth * displayHeight / captureHeight;
            dispHeight = displayHeight;
    
            if (dispWidth > displayWidth)
            {
                dispWidth = displayWidth;
                dispHeight = displayWidth * captureHeight / captureWidth;
            }
    //        dispWidth=1820;
    //        dispHeight=940;
    //		displayWidth=1920;
    //		displayHeight=1080;
    
            pPrm_Video->rtParams.tarWidth = dispWidth;
            pPrm_Video->rtParams.tarHeight = dispHeight;
            pPrm_Video->rtParams.posX = (displayWidth - dispWidth) / 2U;
            pPrm_Video->rtParams.posY = (displayHeight - dispHeight) / 2U;
    
            pPrm_Video->displayId = DISPLAY_LINK_INST_DSS_VID1;
        }
    }
    
    Void chains_network_isp_display_SetIspConfig(chains_network_isp_displayAppObj *pObj)
    {
        appSetDefaultIspParams(&pObj->appSensInfo);
        appSetIspParamsFromDCC(&pObj->appSensInfo);
    }
    
    Void chains_network_isp_display_setMuxes(
    		chains_network_isp_displayAppObj *pObj)
    {
        /* Setup PinMux */
        ChainsPlatform_SetPinMux(pObj->chainsCfg->sensorName);
    
        /* Init Board Mux */
        ChainsBoard_SetBoardMux(pObj->chainsCfg->sensorName);
    }
    
    
    Void chains_network_isp_display_load_network_raw_config(chains_network_isp_displayAppObj *pObj)
    {
    	LoadNetworkRawFramesOption(pObj->enable_network_raw_frames);
    		if(0 == strcmp("ON", pObj->enable_network_raw_frames))
    		{
    			pObj->ucObj.NetworkRxPrm.enable_network_raw_frames=1;
    		}
    		else if(0 == strcmp("OFF", pObj->enable_network_raw_frames))
    		{
    			pObj->ucObj.NetworkRxPrm.enable_network_raw_frames=0;
    		}
    		else
    		{
    			pObj->ucObj.NetworkRxPrm.enable_network_raw_frames=0;
    		}
    
    
    }
    
    
    Void chains_network_isp_display_SetAppPrms(chains_network_isp_displayObj *pUcObj,
                                       Void *appObj)
    {
    
    	UInt32 chId;
    	System_LinkChInfo *pChInfo;
    	chains_network_isp_displayAppObj *pObj = (chains_network_isp_displayAppObj *)appObj;
    	chains_network_isp_display_load_network_raw_config(pObj);
    
    	pUcObj->IssM2mIspPrm.channelParams[0].inBpp=SYSTEM_BPP_BITS16;
    	pUcObj->IssM2mIspPrm.channelParams[1].inBpp=SYSTEM_BPP_BITS16;
    	pUcObj->IssM2mIspPrm.channelParams[2].inBpp=SYSTEM_BPP_BITS16;
    	pUcObj->IssM2mIspPrm.channelParams[3].inBpp=SYSTEM_BPP_BITS16;
    
    	Vps_printf("the value is %d",pUcObj->NetworkRxPrm.enable_network_raw_frames);
    	for (chId = 0; chId < pUcObj->NetworkRxPrm.outQueInfo.numCh; chId++)
    	{
    	  pChInfo = &pUcObj->NetworkRxPrm.outQueInfo.chInfo[chId];
    	  if(pUcObj->NetworkRxPrm.enable_network_raw_frames==1)
    	  {
    		  pChInfo->flags = System_Link_Ch_Info_Set_Flag_Data_Format(pChInfo->flags,SYSTEM_DF_BAYER_RGGB);
    	  }
    	}
    
    
        ChainsCommon_GetDisplayWidthHeight(pObj->chainsCfg->displayType,
                                           &pObj->displayWidth, &pObj->displayHeight);
    
        pUcObj->IPCOut_A15_0_IPU1_0_0LinkID
                = SYSTEM_MAKE_LINK_ID(
                    pObj->netProcId,
                    pUcObj->IPCOut_A15_0_IPU1_0_0LinkID);
    
            pUcObj->NetworkRxLinkID
                = SYSTEM_MAKE_LINK_ID(
                    pObj->netProcId,
                    pUcObj->NetworkRxLinkID);
    
            pObj->captureOutWidth  = NETWORK_RX_FRAME_WIDTH;
            pObj->captureOutHeight = NETWORK_RX_FRAME_HEIGHT;
    
    
        /* Create the sensor now */
        strncpy(pObj->appSensInfo.sensorName, pObj->chainsCfg->sensorName,
                ISS_SENSORS_MAX_NAME);
        pObj->appSensInfo.numCh = 1;
        pObj->appSensInfo.ispOpMode = pObj->chainsCfg->ispOpMode;
        //pObj->appSensInfo.numCSI2Inst = 1;
        appCreateISSSensor(&pObj->appSensInfo);
    
    
        ChainsCommon_SetNetworkRxPrms_ND(
                   &pUcObj->NetworkRxPrm,
                   pObj->captureOutWidth,
                   pObj->captureOutHeight,
                   1,
                   30
               );
    
        appInitIssIspParams(&pObj->appSensInfo, pUcObj->IssM2mIspLinkID,
                            &pUcObj->IssM2mIspPrm);
        appInitIssAewbParams(&pObj->appSensInfo, pUcObj->Alg_IssAewbLinkID,
                             &pUcObj->Alg_IssAewbPrm);
    
        pUcObj->IssM2mIspPrm.allocBufferForDump = TRUE;
    
        ChainsCommon_SetGrpxSrcPrms(&pUcObj->GrpxSrcPrm,
                                                       pObj->displayWidth,
                                                       pObj->displayHeight
                                                      );
    
        ChainsCommon_SetDisplayPrms(&pUcObj->Display_VideoPrm,
                                        &pUcObj->Display_GrpxPrm,
                                        pObj->chainsCfg->displayType,
                                        pObj->displayWidth,
                                        pObj->displayHeight
                                       );
    
        chains_network_isp_display_SetDisplayPrms(
                &pUcObj->Display_VideoPrm,
                pObj->chainsCfg->displayType,
                pObj->displayWidth, pObj->displayHeight,
                pUcObj->IssM2mIspPrm.channelParams[0U].outParams.widthRszA,
                pUcObj->IssM2mIspPrm.channelParams[0U].outParams.heightRszA);
    
        ChainsCommon_StartDisplayCtrl(pObj->chainsCfg->displayType,
                                      pObj->displayWidth, pObj->displayHeight);
    }
    Void ChainsCommon_SetNetworkRxPrms_ND(
                            NetworkRxLink_CreateParams *pPrm,
                            UInt32 maxWidth,
                            UInt32 maxHeight,
                            UInt32 numCh,
                            UInt32 fps /* in msecs */
                            )
    {
        UInt32 chId;
        System_LinkChInfo *pChInfo;
    
        pPrm->outQueInfo.numCh = numCh;
    
        pPrm->timerPeriodMilliSecs = 1000/fps;
    
        for (chId = 0; chId < pPrm->outQueInfo.numCh; chId++)
        {
            pPrm->channelParams[chId].numBuffers = 6;
    
            pChInfo = &pPrm->outQueInfo.chInfo[chId];
    
    
    
            pChInfo->flags = System_Link_Ch_Info_Set_Flag_Scan_Format(pChInfo->flags,
                                                        SYSTEM_SF_PROGRESSIVE);
            pChInfo->width = maxWidth;
            pChInfo->height = maxHeight;
            pChInfo->startX = 0;
            pChInfo->startY = 0;
            pChInfo->pitch[0] = SystemUtils_align(pChInfo->width, 32);
            pChInfo->pitch[1] = SystemUtils_align(pChInfo->width, 32);
    
        }
    
        pPrm->networkServerPort = NETWORK_RX_SERVER_PORT;
        /* Select network mode for null source link */
        ChainsCommon_networkRxSetMode(pPrm);
    
    
    }
    Void chains_network_isp_display_StartApp(chains_network_isp_displayAppObj *pObj)
    {
        Chains_memPrintHeapStatus();
        chains_network_isp_display_SetIspConfig(pObj);
        chains_network_isp_display_setMuxes(pObj);
        appStartIssSensorSerDes(&pObj->appSensInfo);
        ChainsCommon_StartDisplayDevice(pObj->chainsCfg->displayType);
        chains_network_isp_display_Start(&pObj->ucObj);
        Chains_prfLoadCalcEnable(TRUE, FALSE, FALSE);
    }
    
    Void chains_network_isp_display_StopAndDeleteApp(chains_network_isp_displayAppObj *pObj)
    {
    	chains_network_isp_display_Stop(&pObj->ucObj);
    	chains_network_isp_display_Delete(&pObj->ucObj);
    
    	chains_network_isp_display_FreeMemory(pObj);
    
        ChainsCommon_StopDisplayCtrl();
    
        appStopISSSensor(&pObj->appSensInfo);
    
        appDeleteISSSensor(&pObj->appSensInfo);
    
        ChainsCommon_StopDisplayDevice(pObj->chainsCfg->displayType);
    
        /* Print the HWI, SWI and all tasks load */
        /* Reset the accumulated timer ticks */
        Chains_prfLoadCalcEnable(FALSE, TRUE, TRUE);
    }
    
    Void chains_network_isp_display(Chains_Ctrl *chainsCfg)
    {
        char ch;
        UInt32 done = FALSE;
        chains_network_isp_displayAppObj* pChainsObj = (chains_network_isp_displayAppObj*)Utils_memAlloc(
        UTILS_HEAPID_DDR_CACHED_SR, sizeof(chains_network_isp_displayAppObj), 16);
        UTILS_assert(pChainsObj != NULL);
        memset(pChainsObj, 0, sizeof(chains_network_isp_displayAppObj));
    
        pChainsObj->netProcId = Utils_netGetProcId();
        UTILS_assert(chainsCfg != NULL);
        strncpy(chainsCfg->sensorName, SENSOR_AR0220, ISS_SENSORS_MAX_NAME);
    
        if (TRUE == IssM2mIspLink_IsWdrMode(chainsCfg->ispOpMode))
        {
            Vps_printf(" chains: Please make sure BSP is build with WDR and LDC "
                       "enabled !!!\n");
        }
    
        pChainsObj->chainsCfg = chainsCfg;
    
        /* Initialize Video Sensor, so that Algorithm can use Params
       from Vid Sensor layer */
        chains_network_isp_display_Create(&pChainsObj->ucObj, pChainsObj);
        chains_network_isp_display_StartApp(pChainsObj);
    
        while (!done)
        {
            Vps_printf(gchains_network_isp_display_runTimeMenu);
    
            ch = Chains_readChar();
    
            switch (ch)
            {
            case '0':
                done = TRUE;
                break;
            case 'p':
            case 'P':
                ChainsCommon_PrintStatistics();
                chains_network_isp_display_printStatistics(&pChainsObj->ucObj);
                break;
            default:
                Vps_printf("\nUnsupported option '%c'. Please try again\n", ch);
                break;
            }
        }
    
        chains_network_isp_display_StopAndDeleteApp(pChainsObj);
    }
    
    
    

    Hi Mayank,

    Did i have to set the DCC in usecase ? I have attched my usecase configuration file for your refernce above.

    Can you please check the file and help in setting the configuration correctly.

    Regards,

    Aneesh

  • Aneesh,

    DCC APIs are called by M2MISP link. The usecase does not need any changes.

    Sensor driver must assign a DCC id and have DCC database included as a header file. Please refer to one of the existing sensor drvers.

    For e.g. AR0233 -> iss_sensor_ar0233.c

    #include "ar0233_dcc.h"

        prms->dccId             = 233U;

    You may start by reusing the DCC header file and ID from an existing sensor. Please pick a sensor which is closes to the RAW files you are providing.

    Regards,

    Mayank

  • Hi Mayank,

    The details you have given are already there in my code, but the sensor is ar0220.

    Still, Its not working perfectly.

    Regards,

    Aneesh

  • Aneesh,

    Couple of suggestions:

    1. Do you have AEWB link in the usecase? If yes, you will need to remove it since that link tries to communicate with an image sensor.

    2. Please check sewbMode in the Sensor Parameters. To be safe, please set it to ALGORITHMS_ISS_AEWB_MODE_NONE

    Regards,

    Mayank

  • 7002.grbg_12b.raw.txt

    Hi Mayank,

    I tried removing the aewb link and tried but there is no improvement. 

    I have attached my input file. Please check it and it is giving out  a grey colour approxmately(R=G=B=128) for your reference.

    If possible give me a input file and tell the expected output of that input, because i am not able to understand where exactly the problem is there wheather the input or configuration.

    Can you please tell  he 1-ch iss capture display usecase  is isscapture_isp_simcop display. or another one.If it is another one can you please give the usecase.

    Is it possile to save the raw data before sending to isp?

    Regards,

    Aneesh

  • Please share the image dimensions for visualization.

    I will suggest you use a real world image or a test pattern captured from the image sensor of your choice. While working with synthetic images it is hard to know the ground truth.

  • Hi Mayank,

    The image dimensions are 1820x940.

    Is it possible to store raw data from camera (Iss Capture)?

    If yes, can you please help me in saving raw bayer data from iss capture .

    I found a link in which it is discussed but i cannot find the usecase(single channel ISS). The forum link is given below.

    https://e2e.ti.com/support/processors/f/791/t/667341?TDA2EG-iss-capture-link-dump-frame-command

    Regards,

    Aneesh

  • I don't have any images from AR0220. Attached is an image from AR0233. The resolution is 1920x1280 and Bayer phase is GRGB

  • orginal.zip

    board output.zip

    Hi Mayank,

    I used the bayer image you have given and i did not got the correct output.

    I have attached the output for your reference and also the original image.

    The output on hdmi is with Aewb off.

    Regards,

    Aneesh

  • Can you please share the ISP output buffer in YUV420SemiPlanar format?

  • isp output.zip

    Hi Mayank,

    The bayer raw image you have sent me is GRBG or GRGB. If it is GRGB then i dont have that format in my code to proceess.

    If it is GRBG then the ISPoutput buffer is attached above.

    Regards,

    Aneesh

  • The raw image is 1920x1280. Are you processing it with the same settings?

  • Hi Mayank,

    I cropped the image to 1920*1080 and used it.

    Regards,

    Aneesh

  • Can you please share the cropped Bayer image?

    Please also elaborate on how you are configuring the ISP for 1920x1080.

  • grbg_16b_1080.zip

    Hi Mayank,

    I have attched the cropped bayer image.

    About configuration, I have changed the resolutions to 1920x1080 in sensor parameters.

    I have given the sensor parameters for your reference.

    IssSensorIf_Params *prms = &SensorParams_Ar0220;
    IssSensor_Info *info = &SensorParams_Ar0220.info;

    IssSensorIf_Params_Init(prms);
    strncpy(prms->name, SENSOR_AR0220, ISS_SENSORS_MAX_NAME);

    prms->dccId = 233U;
    info->width = 1920;
    info->height = 1280;
    info->dataFormat = SYSTEM_DF_BAYER_GRBG;
    info->bpp = SYSTEM_BPP_BITS12;
    info->features = ISS_SENSORS_AR0220_FEATURES;
    info->aewbMode = ALGORITHMS_ISS_AEWB_MODE_AEWB;
    info->maxExp = 1;
    info->ramOffset = 24*1024*1024;

    prms->start = AR0220_Start;
    prms->stop = AR0220_Stop;
    prms->setAeParams = AR0220_SetAeParams;
    prms->getExpParams = AR0220_GetExpParams;
    prms->getDccParams = AR0220_GetDccParams;
    prms->initAewbConfig = AR0220_InitAewbConfig;
    prms->getIspConfig = AR0220_GetIspConfig;
    prms->readWriteReg = AR0220_ReadWriteReg;

    and also i am changing the height and width values of the network_tx tool and network rx.

    Thanks and Regards

    Aneesh

  • nfo->width = 1920;
    info->height = 1280;

    Why is the height 1280?

  • Hi Mayank,

    Sorry for that i just changed that before for testing  i sent that to you. The isp output i have sent is with 1920x1080 .

    Regards,

    Aneesh

  • Aneesh,

    ISP output looks garbled up. It is not clear where it is getting corrupted. A few suggestions:

    1. Double check that the networking layer is sending the image correctly.

    2. If you have LDC in your usecase, please disable it.

    3. Dump the ISP input and output images from the function IssM2mIspLink_drvProcessFrame. You will need CCS and a JTAG.

  • As discussed on Dec-12-2019, the wrong output was caused by incorrect pitch in the network utility used to send the RAW image. After correcting the pitch, Harman is able to get the correct output from ISP.

    It was agreed that this thread can be closed.