Part Number: PROCESSOR-SDK-TDAX
Other Parts Discussed in Thread: DS90UB960-Q1
Hi,
I have questions regarding 8MP sensor support on TDA4x.
As I read in the TRM, the TDA4x is compliant to MIPI D-PHY standard v1.2 and the Camera Streaming Interface Receiver (CSI_RX_IF) is MIPI CSI-2 v2.0.
I beleive it should be capable to recieive the data from one 8MP camera @ 22 frames per seconds without any issues.
However, In the TRM it is mentioned on page-35, Camera Streaming Interface Receiver (CSI_RX_IF)
- Supports one 4MP camera or eight 2MP camera streams
- Two VP 32-bit streams to VISS inputs of VPAC image processing accelerator
I need some clarification here,
1. What is the frame rate for 4MP camera refered to in TRM ?
2. Does it mean that a single stream from 8MP camera will not be supported ?
2. Due to which limitation only one 4MP camera stream is supported ? Is this limitation only due to the FPD link-III DS90UB960-Q1 Deserielizer on the fusion board ?
3. Is there limitations with the VPAC (VISS) module which is limiting the input to 4MP @ ___ framerate ?
Best regards,
Vivek