Other Parts Discussed in Thread: AM3517
Am I correct in assuming there is no reliable workaround for the EHCI suspend/resume issue with a SMSC USB3320 PHY?
I am still seeing issues with the A8_1.00 release.
I see SDOCM00069781 is marked as fixed (but how it can be found and fixed in the same release I don't know) but there are still a lot of suspend/resume issues still open.
I am aware of the PHY not comming out of suspend issue but it is not clear if this is a PHY issue or if the EHCI controller is just not issuing compatable timing.
My platform uses a USB3320 and i have control over the PHY's RESET and power. I would think this could be made to work if by only doing a brute force reset??
Is this still an active issue?