Hello,
I am trying to use McBSP2 as UART using the instructions given in spra633 (spra633c.zip) on DSK6416 with 5-6k interface. I have connected pins 9, 11, 13 on J15 on 5-6k interface board. I have set the CLKGDV value to 135 to allow 115200 mbps. I have also routed the mcbsp2 off board by setting particular bit in CPLD register (60000006, 7/8).
I get the 'Transmit Completed' message but the receiving part does not work. The program does not stop.
Any issues with this? Any McBSP2 setting I am missing? I have uesed J16 connected on 5-6k interface board for a AD card and that works fine.
Thanks for the help.
Best Regards,
Basu