Part Number: TMDXICE110
Hi again guys,
I'm getting a few errors when compiling the example profinet_slave_IRT_AMIC11x_arm together with the PROFINET stack from Molex.
I'm not sure where it's comming from. It is there somebody who did adapt the stack before?
invalid operands to binary % (have 'void *' and 'unsigned int') Lines59 and 61
invalid operands to binary / (have 'void *' and 'unsigned int') Lines59 and 61
C:\ti\bios_6_73_00_12\packages\gnu\targets\arm\libs\install-native\arm-none-eabi\include\sys\select.h
Line59: # define FD_SET(n, p) ((p)->fds_bits[(n)/NFDBITS] |= (1L << ((n) % NFDBITS)))
Line60: # define FD_CLR(n, p) ((p)->fds_bits[(n)/NFDBITS] &= ~(1L << ((n) % NFDBITS)))
Line61: # define FD_ISSET(n, p) ((p)->fds_bits[(n)/NFDBITS] & (1L << ((n) % NFDBITS)