This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H14: IBIS models

Part Number: 66AK2H14

Hello

When looking at the IBIS model, one can see that several models can be selected for one given pin.

For example MDCLK pin AP31 can be modeled as BC181540_40CCLASS_1P8, or BC181540_40ECLASS_1P8, or BC181540_40DCLASS_1P8.

Since I could nod find any hardware input to select the driver strength (the Shannon had SLRATE input pins), I wonder if there is a mapped register  inside the chip that makes the selection possible (as for DDR3 interface for example) ? and where ?

If not, which model should be used for simulation ?

With best regards,

Bruno