Hi,
Using the C6678 SoC, can be mapped many system events (CIC inputs) to the same host event (CIC outputs)?
Example:
CIC0: can be mapped <EDMA3CC0 TC_ERRINT0> and <EDMA3CC0 TC_ERRINT1> to the same <CIC0_OUT(32+0+11*n) Or CIC1_OUT(32+0+11*(n-4))> ?
Thank you.