Part Number: AM3359
Hello TI,
I have two boards, both have PRP configured, also both have linuxptp installed.
I followed the document "
and able to run ptp4l in prp mode using prp0.cfg file. Both board work fine as one grandmaster and another is ordinary clock. But when I connect both the prp ports to router everything other than ptp work fine. Below are the outputs
When only one port is connected of both boards to network.
ptp4l[8308.071]: master offset 5 s2 freq +1838 path delay 16181 ptp4l[8309.072]: master offset 161 s2 freq +1996 path delay 16188 ptp4l[8310.072]: master offset 7 s2 freq +1890 path delay 16194 ptp4l[8311.072]: master offset -22 s2 freq +1863 path delay 16188 ptp4l[8312.072]: master offset -46 s2 freq +1833 path delay 16194 ptp4l[8313.072]: master offset -229 s2 freq +1636 path delay 16194 ptp4l[8314.073]: master offset 199 s2 freq +1995 path delay 16194 ptp4l[8315.073]: master offset 164 s2 freq +2020 path delay 16212 ptp4l[8316.075]: master offset 89 s2 freq +1994 path delay 16212 ptp4l[8317.075]: master offset -210 s2 freq +1722 path delay 16212 ptp4l[8318.075]: master offset 7 s2 freq +1876 path delay 16212 ptp4l[8319.076]: master offset 53 s2 freq +1924 path delay 16208 ptp4l[8320.076]: master offset -100 s2 freq +1787 path delay 16183 ptp4l[8321.078]: master offset 78 s2 freq +1935 path delay 16194 ptp4l[8322.078]: master offset -95 s2 freq +1785 path delay 16183 ptp4l[8323.077]: master offset -18 s2 freq +1834 path delay 16160 ptp4l[8324.078]: master offset 161 s2 freq +2007 path delay 16157 ptp4l[8325.078]: master offset -17 s2 freq +1878 path delay 16157 ptp4l[8326.079]: master offset -169 s2 freq +1720 path delay 16170 ptp4l[8327.079]: master offset 12 s2 freq +1851 path delay 16170 ptp4l[8328.080]: master offset 6 s2 freq +1848 path delay 16158 ptp4l[8329.082]: master offset 393 s2 freq +2237 path delay 16148 ptp4l[8330.083]: master offset -67 s2 freq +1895 path delay 16148 ptp4l[8331.083]: master offset -197 s2 freq +1745 path delay 16148 ptp4l[8332.083]: master offset 81 s2 freq +1964 path delay 16155 ptp4l[8333.082]: master offset 19 s2 freq +1926 path delay 16164 ptp4l[8334.084]: master offset -120 s2 freq +1793 path delay 16171 ptp4l[8335.083]: master offset -103 s2 freq +1774 path delay 16155
This is what I get as soon as I connect second port of grandmaster or ordinary clock.
ptp4l[8401.113]: master offset 28 s2 freq +1910 path delay 16184 ptp4l[8402.114]: master offset -95 s2 freq +1796 path delay 16184 ptp4l[8403.114]: master offset -64 s2 freq +1798 path delay 16181 ptp4l[8404.115]: master offset 134 s2 freq +1977 path delay 16181 ptp4l[8405.115]: master offset 7 s2 freq +1890 path delay 16184 [ 8405.407554] prueth pruss_eth eth0: Link is Up - 100Mbps/Full - flow control rx/tx ptp4l[8405.494]: timed out while polling for tx timestamp ptp4l[8405.494]: increasing tx_timestamp_timeout may correct this issue, but it is likely caused by a driver bug ptp4l[8405.495]: port 3: send peer delay response failed ptp4l[8405.495]: port 3 (eth1): SLAVE to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED) ptp4l[8405.526]: port 2: link up ptp4l[8405.538]: red port 2 (eth0): FAULTY to LISTENING on INIT_COMPLETE ptp4l[8406.116]: port 2: new foreign master 2c6b7d.fffe.49e929-3 ptp4l[8406.547]: red port 3 (eth1): FAULTY to LISTENING on INIT_COMPLETE ptp4l[8406.549]: port 3 lanid=1: rogue peer delay response ptp4l[8406.551]: port 3 (eth1): LISTENING to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED) ptp4l[8407.567]: red port 3 (eth1): FAULTY to LISTENING on INIT_COMPLETE ptp4l[8408.117]: port 3: new foreign master 2c6b7d.fffe.49e929-3 ptp4l[8408.120]: selected best master clock 2c6b7d.fffe.49e929 on port 2 ptp4l[8408.120]: selected best master clock 2c6b7d.fffe.49e929 ptp4l[8408.120]: red port 2 (eth0): LISTENING to UNCALIBRATED on RS_SLAVE ptp4l[8409.576]: port 2 lanid=0: rogue peer delay response ptp4l[8409.581]: port 2 (eth0): UNCALIBRATED to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED)
My current config file is
[global] sanity_freq_limit 0 step_threshold 0.00002 tx_timestamp_timeout 10 domainNumber 0 priority1 128 priority2 123 slaveOnly 0 twoStepFlag 1 summary_interval 0 doubly_attached_clock 1 [prp0] redundancy 2 delay_mechanism P2P network_transport L2 [eth2] redundancy 2 redundancy_master_interface prp0 redundancy_slave_number 1 logAnnounceInterval 0 logSyncInterval 0 logMinPdelayReqInterval 0 announceReceiptTimeout 3 syncReceiptTimeout 2 delay_mechanism P2P egressLatency 726 ingressLatency 186 network_transport L2 fault_reset_interval 0 [eth3] redundancy 2 redundancy_master_interface prp0 redundancy_slave_number 2 logAnnounceInterval 0 logSyncInterval 0 logMinPdelayReqInterval 0 announceReceiptTimeout 3 syncReceiptTimeout 2 delay_mechanism P2P egressLatency 726 ingressLatency 186 network_transport L2 fault_reset_interval 0
I run command on master ptp4l -f <path to prp0.cfg> -m
Also on slave ptp4l -f <path to prp0.cfg> -m -s