Part Number: AM5718
SDK : ti-processor-sdk-linux-rt-am57xx-evm-05.03.00.07
u-boot : u-boot-2018.01+gitAUTOINC+313dcd69c2-ge2bc936055
kernel : linux-rt-4.14.79+gitAUTOINC+a72bf1418c-ga72bf1418c
------------------------------------------------------------------------------------------
I have a problem with rgmii now.
After using eth0, if you use the ethernet cable used for eth0 to eth1, it will not work. However, if you type and use "ifconfig eth0 down", it is enabled.
Do you know the cause?
I am using am5718 custom board.