This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2SX: TDA2X - Continuous attaching message after algorithm added

Part Number: TDA2SX


Hello,

I wanted to run TIDL_preproc algorithm on DSP and in order to do that I modified vision_sdk_usecase_gen (link.cpp) to enable TIDL_preproc to run on DSP. I generated usecase with TIDL preproc running od DSP, added initPlugin for TIDL_preproc in app_init_dsp.c and build was successful. I updated rootfs on sd card with files from /lib/firmware folder and with apps.out file. When I run usecase I got continuous messages of trying to attach cores to IPU2.

[HOST] [IPU2  ]     49.452571 s:  SYSTEM: Attaching to [DSP1] ...
 [HOST] [DSP2  ]     50.369669 s:  SYSTEM: Attaching to [IPU2] ...
 [HOST] [IPU2  ]     50.452601 s:  SYSTEM: Attaching to [DSP1] ...
 [HOST] [DSP2  ]     51.369700 s:  SYSTEM: Attaching to [IPU2] ...
 [HOST] [IPU2  ]     51.452601 s:  SYSTEM: Attaching to [DSP1] ...
 [HOST] [DSP2  ]     52.369730 s:  SYSTEM: Attaching to [IPU2] ...
 [HOST] [IPU2  ]     52.452632 s:  SYSTEM: Attaching to [DSP1] ...
 [HOST] [DSP2  ]     53.369761 s:  SYSTEM: Attaching to [IPU2] ...
 [HOST] [IPU2  ]     53.452662 s:  SYSTEM: Attaching to [DSP1] ...
 [HOST] [DSP2  ]     54.369761 s:  SYSTEM: Attaching to [IPU2] ...
 [HOST] [IPU2  ]     54.452693 s:  SYSTEM: Attaching to [DSP1] ...
 [HOST] [DSP2  ]     55.369791 s:  SYSTEM: Attaching to [IPU2] ...
 [HOST] [IPU2  ]     55.452723 s:  SYSTEM: Attaching to [DSP1] ...
 [HOST] [EVE1  ]     55.460287 s:  SYSTEM: Attaching to [IPU2] ...
 [HOST] [EVE2  ]     55.460287 s:  SYSTEM: Attaching to [IPU2] ...
 [HOST] [EVE3  ]     55.460287 s:  SYSTEM: Attaching to [IPU2] ...
 [HOST] [EVE4  ]     55.460287 s:  SYSTEM: Attaching to [IPU2] ...
 [HOST] [DSP2  ]     56.369822 s:  SYSTEM: Attaching to [IPU2] ...
 [HOST] [IPU2  ]     56.452754 s:  SYSTEM: Attaching to [DSP1] ...
 [HOST] [DSP2  ]     57.369852 s:  SYSTEM: Attaching to [IPU2] ...
 [HOST] [IPU2  ]     57.452784 s:  SYSTEM: Attaching to [DSP1] ...

P.S. I am using Linux+RTOS configuration and PSDK version 3.04.00.00.

Regards,
Sasa