Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hi,
I am using OMAP-L138 EVM from Logic PD.
If my understanding is correct now Logic PD EVM supports flashing the bootloader through UART2.
We are in the process of designing HW in which we are planning to use UART1 for boot mode.
With this change my understanding is that I need to generate a new AIS file using AISgen for D800K006 right and I have to select BOOT mode as UART1 is my understanding correct ?
And to program the SPI Flash using SFH we need to set the S7-7 and S7-8 to ON. With this OMAP-L138 enters in UART2 Boot mode right?
The WinCE BSP Install BSP_WINCE_ARM9_01_00_01\PLATFORM\OMAPL138_AM18X\SRC\BOOT\TOOLS\bin contains the arm-spi-ais.bin for generating this what is ARM application file?
Thank You & Regards,
GSR