Hi,
I am trying to import and run inference using binary file as input data.
It's fine in the import phase.
When running the inference by run ./PC_dsp_test_dl_algo.out.
Here's the error message:
Error at line: 208 : in file src/tidl_tb.c, of function : tidl_tb_algCreate
Error Type: TIDL_E_QUANT_STATS_NOT_AVAILABLE
Error at line: 479 : in file src/tidl_tb.c, of function : tidlMultiInstanceTest
Error Type: TIDL_E_QUANT_STATS_NOT_AVAILABLE
---------------------------------------------------------------------------------------------------------------------------------------
Import.txt
modelType = 0
inputNetFile = "../../test/testvecs/models/public/caffe/test/Model.prototxt"
inputParamsFile = "../../test/testvecs/models/public/caffe/test/Model.caffemodel"
outputNetFile = "../../test/testvecs/config/tidl_models/caffe/tidl_net_mm.bin"
outputParamsFile = "../../test/testvecs/config/tidl_models/caffe/tidl_io_mm"
inElementType = 0
inFileFormat = 1
perfSimConfig = ../../test/testvecs/config/import/perfsim_base.cfg
tidlStatsTool = ../../test/tidl_quant_stats_tool.out
inData = ../../test/testvecs/input/input.bin
postProcType = 0
foldMaxPoolInConv2D = 0
---------------------------------------------------------------------------------------------------------------------------------------
inference.txt
inFileFormat = 1
postProcType = 0
padInBuffInTB = 1
netBinFile = "testvecs/config/tidl_models/caffe/oToBrite/tidl_net_mm.bin"
ioConfigFile = "testvecs/config/tidl_models/caffe/oToBrite/tidl_io_mm1.bin"
outData = testvecs/output/out.bin
inData = testvecs/input/input.bin
totNumClasses = 8
debugTraceLevel = 3
writeTraceLevel = 3
---------------------------------------------------------------------------------------------------------------------------------------
Is there any mistake I have made in my import.txt or infer.txt?
Thank you.