Hello,
We're designing a custom board with two 6474's and one 6455 on it. In the first 6474 we want to use I2C Boot for the initial bootcode, then use an SPI Flash for the system load.
Then I want to use SRIO Boot for the other 6474 and 6455.
My question is, I think SRIO Port 0 must be used for the SRIO boot mode, but since I don't want to use an SRIO Switch, I will connect Master 6474 SRIO 0 to Second 6474 SRIO 0 and Master DSP SRIO 1 to 6455 SRIO 0. Can I use this setup for boot of the other DSP over SRIO links?
Thanks
Alphan