Other Parts Discussed in Thread: OMAP-L138
Hi,
The version of my linux kernel is 2.6.32-rc6, once I connect my 320G harddisk with OMAP-L138, the format of the disk is FAT32,and the sata interface worked well. Then I try to connect my 1T harddisk with OMAP-L138, but it cannot reset sucessfully, the following are the warnings:
ata1: link is slow to respond, please be patient (ready=0)
ata1: softreset failed (device not ready)
ata1: link is slow to respond, please be patient (ready=0)
ata1: softreset failed (device not ready)
ata1: link is slow to respond, please be patient (ready=0)
ata1: softreset failed (device not ready)
ata1: limiting SATA link speed to 1.5 Gbps
ata1: softreset failed (device not ready)
ata1: reset failed, giving up
Then I change the format of my 1T harddisk from NTFS to FAT32, but it cannot work either. Then I put a 500G hardisk (NTFS) in the harddisk case and then connect it with OMAP-L138,I got the following direction:
scsi 1:0:0:0: Direct-Access WDC WD50 00BEVT-22A0RT0 0009 PQ: 0 ANSI: 0
sd 1:0:0:0: [sda] Spinning up disk...Please wait: booting...
Starting udev
..
udev: starting version 141
.ready
sd 1:0:0:0: [sda] 976773164 512-byte logical blocks: (500 GB/465 GiB)
sd 1:0:0:0: [sda] Write Protect is off
sd 1:0:0:0: [sda] Assuming drive cache: write through
sd 1:0:0:0: [sda] Assuming drive cache: write through
sda: sda1 sda2 sda3 sda4
sd 1:0:0:0: [sda] Assuming drive cache: write through
sd 1:0:0:0: [sda] Attached SCSI disk
But when I login, then use the mount direct to mount the sda device to /mnt,it does not work.
Is this a problem of my linux kernel driver or the format of the harddisk, or the own limitation of OMAP-L138.
Looking forward to your advice.
regars
XingwangXu