This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using Windows host instead of Linux host for DM6467T EVM development (aka Spectrum Digital HD1080P)



(Please note that this is a breakout thread from http://e2e.ti.com/support/embedded/f/356/p/86363/298144.aspx#298144)

I currently have multiple Windows PCs but no Linux in house.  After reviewing my roadmap at http://e2e.ti.com/support/embedded/f/356/p/86363/298144.aspx#298144, are there any things I'll be needing to do that really REQUIRE Linux?

For example, can I change boot methods using a Windows PC?  The wiki at http://processors.wiki.ti.com/index.php/GSG:_DM6467_DVEVM_Additional_Procedures#Alternate_Boot_Methods gives only Linux instructions (and doesn't give instructions at all for NAND file system).

Thanks,

Helmut