Hi,
A power failure occurred in a customer's product using TMS320C6748.
Upon reviewing the symptoms, it was very similar to Advisory 2.3.18 of TMS320C6748 errata.
They want to try the workaround.
There were some questions about workarounds.
It is understood that Workaround (a) suppresses the amount of current to 140 mA or less with a capacitor. We can't understand this.
Capacitors charge and discharge, and they think the problem cannot be solved by the OFF time, but why is adjustment with capacitors?
*********Work around (a)*********
Maintain sufficient bulk capacitance on the DVDD18 supply such that the charging current for these capacitors provides all or part of the required >140 mA. Bulk capacitance in this context means the total capacitance seen by the DVDD18 supply (filter capacitors, bypass capacitors, etc.). Capacitor charging current is defined as I = C*(dV/dt).
So the ramp rate of the DVDD3318_x supply and the total bulk capacitance on the DVDD18 supply can be used to calculate the current produced.
This solution provides additional power supply filtering and little current leakage after the supplies are ramped (depending on the type of capacitors used). The table below shows some examples of the bulk capacitance that would be required to use this solution alone:
*********Work around (a)*********
Question 1:
Please let me know a little more.
Question 2:
If State is error state (Error state of the IO buffer during Zone G)
How does C6748 behave?
Will it break? Does it not work according to the characteristics of DS?
Regards, Rei