Hello,
I run a case on mcu1_0, now I want to add a gpio interrupt for test,do you have an example for gpio interrupt configure?
Thanks.
Qin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Qin,
Please refer to example pdk\packages\ti\drv\gpio\test\led_blink\src\main_led_blink.c in PDK for GPIO example. This GPIO blinks some LEDs on EVM.
Rgds,
Brijesh
Dear Brijesh,
I run the GPIO example on J721E EVM,and it looks normal through the log,but I didn't see some LEDs blink on the board.
then I add a log in the callback function,as a result,it didn't go to the callback function.what? the interrupt isn't be triggered? How should I do to verify it?
Thanks,
Qin
Hi Qin,
Are you looking for interrupt? Does polling mode work fine?
Rgds,
Brijesh
Hi Qin,
I think we need to configure Interrupt router and Aggregator to get interrupt.
Let me check and tell you exact steps required.
Rgds,
Brijesh
Hi,
This thread is being discussed over email, so closing it here.
Rgds,
Brijesh
Hi Brijesh,
I have the same problem here: Maybe you could share here the information/ exact steps which are required?
Thank you very much!
Best regards,
Thomas
Hi Thomas,
Which GPIO are you trying to enable? Are you using GPIO driver to enable it?
Rgds,
Brijesh
I try to enable GPIO0_124, since its connected to J5:20 on the GESI expansion board.
I configured it as output which works. I did this with GPIO driver.
Now I want to configure it as interrupt source, but this does not work. I am confused how the GPIO driver works, and which information I need to get it working. I just want to trigger a function of RTOS when a interrupt was detected on that GPIO0_124.
Brijesh,
I tracked my error down but need nevertheless some assistance, as you can see here: 
However, If I use this GPIO API, I can see that the bit for GPIO0_124 interrupt is set in register GPIO_INTSTAT67, but my registered ISR is not called:
void someCallbackFunction(void)
{
volatile int foobar = 0;
foobar++;
System_printf("INTERRUPT OCCURED!!!!!!!!!\n");
return;
}
/* GPIO Driver board specific pin configuration structure */
GPIO_PinConfig gpioPinConfigs[] =
{
/* Input pin with interrupt enabled */
GPIO_DEVICE_CONFIG(0, 124) | GPIO_CFG_OUTPUT,
};
/* GPIO Driver call back functions */
GPIO_CallbackFxn gpioCallbackFunctions[] =
{
NULL,
};
/* GPIO Driver configuration structure */
GPIO_v0_Config GPIO_v0_config =
{
gpioPinConfigs,
gpioCallbackFunctions,
sizeof(gpioPinConfigs) / sizeof(GPIO_PinConfig),
sizeof(gpioCallbackFunctions) / sizeof(GPIO_CallbackFxn),
#ifdef __TI_ARM_V7R4__
0x8U
#else
#if defined(__C7100__)
0x01U
#else
0x20U
#endif
#endif
};
int initCustomGpio()
{
GPIO_v0_HwAttrs gpio_cfg;
GPIO_socGetInitCfg(0, &gpio_cfg); // 0 = GPIO_LED0_PORT_NUM
GPIO_socSetInitCfg(0 /*GPIO PORT NUM*/, &gpio_cfg);
//After configuration, init GPIO modules
GPIO_init();
//Set callback function and then enable interrupt
GPIO_setCallback(0, (GPIO_CallbackFxn)&someCallbackFunction);
GPIO_enableInt(0);
GPIO_write(0, 0);
GPIO_write(0, 1);
GPIO_write(0, 0);
}
Maybe you could give me feedback, if I use the GPIO API here in a correct way.
I think a lean and clean documentation from TI, how to use GPIO driver properly would helped me and other people a lot, which are new to TI SoCs.
The overloaded/overcrowded GPIO blink led example does not help at all (at least for me). It's more confusing and frustrating digging to all the symbol defines to get a connection between the required GPIO register name values and TRM documentation.
Hi Thomas,
I think you are providing the interrupt number. Please refer to GPIO_configIntRouter API in pdk\packages\ti\drv\gpio\test\led_blink\src\main_led_blink.c to understand ow to provide interrupt number to GPIO driver.
Rgds,
Brijesh
Hi Brijesh,
I looked at main_led_blink.c example, but don't know how to configure the interrupt controller and interrupt router for executing a HWI on mcu2_0 with RTOS from interrupt by GPIO0_124.
I ran the examples "GPIO_LedBlink_j721e_evm_mcu1_0TestApp_debug.xer5f" and "GPIO_Baremetal_LedBlink_j721e_evm_mcu1_0TestApp_debug.xer5f" on my TDA4VMXEVM, which both don't work. No LED is blinking on my board (Anyway, which LEDs should blink?).
My current state is, that the GPIO0 module is configured in a correct way. I can see at the specific GPIO0 registers that the interrupt got successfully detected.
Now I have to route this interrupt signal to mcu2_0 VIM (I think at least).
This is what I puzzled from the TRM:
1. GPIO_0_INT124 is connected to interrupt router "GPIOMUX_INTRTR0"
2. GPIO_0_INT124 corresponds to GPIO0 Bank 7. (9.4.3.16) GPIOMUX_INTRTR0 Interrupt Map shows that GPIO0_GPIO_BANK7 is mapped to GPIOMUX_INTRTR0_IN_263.
(Table 9-200. GPIOMUX_INTRTR0 Interrupt Map)
3. If I look how GPIOMUX_INTRTR0 is integrated into MAIN_DOMAIN, I have no figure in the TRM (Section 9.3.2.2).
What I need to do to route the interrupt from GPIOMUX_INTRT0 to mcu2_0??
Hi Thomas,
We dont really need to explicitly configure interrupt router and controller. We need to use DMSC firmware for this.
Rgds,
Brijesh