Hi
I got a C6A8168 board From kind TI University program. But only main board without SD Card or mouse etc.
By using the EZSDK, I made a boot SD card which contains

Next, according to the Quick start guide,
I did the settings of SW3 and SW4 like these images, connected a UARRT, Ethernet cable, HDMI cable to a TV, 12V-DC power,
insert my SD card with boot files. But no mouse connected.
Finally When I power SW1 on, I got no response to UART, or HDMI TV.
The UART's setting is
Port: COM1
Baud rate: 115200
Data: 8 bits
Parity: none
Stop: 1 bit
Flow control: none
Because this board is new, I can't find much helpful information on the internet.
Your one word may be great help to me.
Regards
SONG Yang