This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS0914: Drivers for SDXDS510USB-Plus not found by the TI nowFlash v3.42.3

Part Number: TMS570LS0914
Other Parts Discussed in Thread: UNIFLASH

When reading or programming request is run through the TI nowFlashWin.exe, the nowFlash.exe is executed and following log appears:
"nowFlash version 3.42 Build <official>
Config file C:\ti\nowflash\v3.42.3\nowFlash.cfg Revision 3
Please force the driver path using the '-dll <driver>' option.
Error 131 - Could not find or load requested emulation driver.
***************************************************
Check that the INSTALL_PATH and DRIVERS paths in the nowFlash.ini file represent valid paths, and that the specified driver exists in these paths.
***************************************************
See nowFlash.pdf for more info
***************************************************
press Enter to exit"

The driver for Spectrum Digital xds510 is installed appropriately and the TI nowFlash application is configured. The SDXDS510USB device is connected. The driver can be found in the device manager version 6.0.999.2 2.40.0.1315.
Other devices (like xds200) and Uniflash work appropriately. The tested nowFlash config works appropriately on other PCs.

What is meaning of forcing the driver path using the "'-dll <driver>' option"?
What other system/Windows configuration may be checked?