This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H14: FEC support on 10GbE?

Part Number: 66AK2H14

Hello,

The 10GbE user's guide mentions in section 2.6 that the Physical Coding Sublayer supports Forward Error Correction (FEC). But section 3.5.9 PCSR Forward Error Correction Register (PCSR_FEC) describes the enable bits as "tbd".

Is this feature supported?

Thank you.


Best regards,
François.

  • Hi Francois,

    I checked both Processor SDK RTOS & Linux SDKs and the PCSR_FEC register is not set in either of them. I believe this has not been implemented in the K2H design. Let me reconfirm this with the design team.

    Also there is no information that this is enabled in the netcp driver:
     

    Best Regards,
    Yordan

  • Hi Yordan,

    Thank you. Indeed, please check with the design team whether this function is in the silicon or not. I would rather suspect that it is there, disabled by default after reset, but has never been tested.


    Best regards,
    François.

  • Hi,

    Sorry for the late response! We are still checking with design team and will update here.

    Regards, Eric

  • Hi,

    Here from the design team: the K2H does support FEC in the PCSR, it need to be enabled in the regs. If using KR it need to be negotiated and then enabled in the regs.

    Regards, Eric