Hi All,
I would like to ask a question on GPIO.
In document SPRU988b, page 22-27, register definition for
- OUT_DATAn
- SET_DATAn
- CLR_DATAn
are listed.
In the output mode, if SET_DATAn and CLR_DATAn are already sufficient to determine the value of the pin, is OUT_DATAn redundant? Why is it still provided?
Another question is on the terminology used in GPIO’s register description:

What does
- Determine
- Driving high
- Driving low
mean, respectively? Again, doesn’t “determine” include “driving high” and “driving low”? Isn’t it redundant?
Thanks,
Zheng