Other Parts Discussed in Thread: SYSBIOS
Hello TI-san,
I am checking the performance of the LDC sample code (m2mSimcopLdcVtnf) for ProcessorSDK 3.7.0.
In the original source code, it was displayed in the "HW Time in msecs" column with 12 ms after running the program.
Also, when I modified the source code (M2mSimcopLdcVtnf_main.c) to use bilinear interpolation,
it was displayed in the "HW Time in msecs" column with 8 ms after running the program.
If Mesh LDC was running at 500MHz, I expected that these processing times would be about half.
Are these processing times correct?
Best regards,
Yudai ISHIBASHI