Part Number: PROCESSOR-SDK-DRA8X
My setup is
- J721EVM
- J721EXSOMG01EVM ( PROC078E2C (001) )
- Common board PROC079E2A (001)
- PSDKRA&PSDKLA:
V06.00.01
I have a problem with Step 4: Load RTOS/baremetal application binaries thru CCS and can’t access to forum for problem solution.
Scripting Console Log:
Initializing .. (Completed)
js:> load ("/opt/psdk_rtos_auto_j7_06_00_01_00/pdk/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/launch.js");
Connecting to DMSC_Cortex_M3_0!
Loading DMSC Firmware ... /opt/psdk_rtos_auto_j7_06_00_01_00/pdk/packages/ti/drv/sciclient/soc/V1/ti-sci-firmware-j721e-gp.bin
DMSC Firmware Load Done...
DMSC Firmware run starting now...
Connecting to MCU Cortex_R5_0!
Running the board configuration initialization from R5!
Connecting to DMSC_Cortex_M3_0!
Loading DMSC Firmware ... /opt/psdk_rtos_auto_j7_06_00_01_00/pdk/packages/ti/drv/sciclient/soc/V1/ti-sci-firmware-j721e-gp.bin
DMSC Firmware Load Done...
DMSC Firmware run starting now...
Connecting to MCU Cortex_R5_0!
Running the board configuration initialization from R5!
Error loading "/opt/psdk_rtos_auto_j7_06_00_01_00/pdk/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciclient_ccs_init_mcu1_0_release.xer5f": Timed out after 200000ms while waiting for target to halt after an auto-run to "main (/opt/psdk_rtos_auto_j7_06_00_01_00/pdk/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/launch.js#125) (/opt/psdk_rtos_auto_j7_06_00_01_00/pdk/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/launch.js#125)
js:>
Console Log:
DEBUGSSM_0: GEL Output: Configuring ATCM for the R5Fs
DEBUGSSM_0: Trouble Writing Memory Block at 0x45a50100 on Page 0 of Length 0x4
DEBUGSSM_0: GEL: Error while executing OnTargetConnect(): Target failed to write 0x45A50100
at *((unsigned int *) (0x45a50000+0x100))=0x888 [J721E_EVM.gel:188]
at Configure_ATCM() [J721E_EVM.gel:87]
at OnTargetConnect()
DMSC_Cortex_M3_0: Failed System Reset: (Error -1001 @ 0x0) Requested operation is not supported on this device. (Emulation package 8.2.2.47)
MCU_Cortex_R5_0: Trouble Removing Breakpoint with the Action "Process CIO" at 0x41c09244: (Error -1066 @ 0x41C09244) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 8.2.2.47)
MCU_Cortex_R5_0: Trouble Removing Breakpoint with the Action "Terminate Program Execution" at 0x41c09f58: (Error -1066 @ 0x41C09F58) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 8.2.2.47)
MCU_Cortex_R5_0: Trouble Removing Breakpoint with the Action "Finish Auto Run" at 0x41c06b4c: (Error -1066 @ 0x41C06B4C) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 8.2.2.47)