This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4379: DCAN triple-sampling error

Part Number: AM4379

Hello,

Is triple-sampling supported for the CAN bus on the am4379?

If I try to configure the CAN bus with triple-sampling on, I get an "Operation not supported" message.

$> ip link set can0 type can bitrate 1000000 triple-sampling on
RTNETLINK answers: Operation not supported

Do I miss a package or a kernel configuration to enable this mode?

Beside of that configuration the CAN bus is working fine.

Kind regards,

Martin