Part Number: DRA72XEVM
Hello,
I'm implementing the memory protection on the C66x DSP side. The memory protection works but in order to have it working I had to copy functionality from the dsp_xmc.h file. That's because the libraries in the pdk_dra7xx_1_0_10/packages/ti/csl/lib/dra72x/c66/release/ are not built with the XMC functions. There are no symbols like DSPXMCSetMPAXSegment or DSPXMCGetFaultAddr in the library.
What's the proper way of accessing those functions? Do I need to use a xdc.useModule('the XMC module name') in the config file? I can't find any module that would do that in the PDK files.
Regards, Michal