This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: Profinet example error

Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: SYSBIOS, AM3359

Hi,

I am building a sample environment for PROFINET at "PRU-ICSS-Profinet_Slave_01.00.03.04".

The environment is as follows:

・PRU-ICSS-Profinet_Slave_01.00.03.04
・processor_sdk_rtos_am335x_5_01_00_11
・ccs_8.1.0.00011
・XDC_TOOLS_VERSION=3.50.07.20
・SYS_BIOS_VERSION=6.73.00.12
・NDK_VERSION=3.40.01.01
・EDMA_VERSION=2.12.05.30

There is no problem with compiling and there is no problem with loading, but the following error occurs and it cannot be started.

------------------------------------------------------
CortxA8: GEL Output: Application load OK!
CortxA8: SemiHosting : File IO Error : fopen() : C:\ti\PRU-IC~2.04\PROTOC~1\PROFIN~1\projects\PROFIN~1\AM335x_release\:semihosting-features : Invalid argument
CortxA8: Unhandled ADP_Stopped exception 0x801AB198
------------------------------------------------------

In the same way, ECAT sample "PRU-ICSS-EtherCAT_Slave_01.00.07.02" has been started, so I think the procedure is correct...

Could you give me some advice this matter?

Thank you for your confirmation.

Best regards,
Eiji