This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDL testbench on target loops "Waiting for sync"

Hi,

I try to run the TIDL standalone testbench on target.

1)  I setup CCS + EVM as decribed in "CCS Setup for J721e". Board jumpers are set to NOBOOT

2) I prepared an SD card and did everything decribed in "Steps to run Sample Application on EVM" from TIDL users guide

As soon as I start the C7x, the debug console repeats constantly "Waiting for sync 82000000, 0". Do I need to start something else? What is going to be synchronized?

Regards

Jan