Other Parts Discussed in Thread: TDA4VM
Hi TI support team
As I know the USB id used for OTG function as switching between host and device/slave mode,
So I add 10K PD for USB0_ID as TDA4VM USB host mode for default because I don’t have usb id pin from usb connector.
But If I want to use TDA4VM DFU boot feature:
- Can I need change USB0_ID status to slave mode for default?
- The USB0_ID signal is open for slave mode?
- Can I add PU from external resistor ? but DM mention should never be connected to any external voltage source.
- Can I need use GPIO to control USB0_ID status ? or only use PD resistor or open for USB0_ID pin.
Thanks
Yutai