Hello. I was able to compile an application compiled with library for QT5.6.1 before, and it ran without a problem on am5718 board.
Then I've made a shared library for SISCO 61850 application and compiled the application with the shared library. (I've run a simple test code with the shared library, so there is no problem with producing the library)
The application is not starting with these error messages below.
QIconvCodec::convertToUnicode: using Latin-1 for conversion, iconv_open failed
QIconvCodec::convertFromUnicode: using Latin-1 for conversion, iconv_open failed
Unable to figure out framebuffer device. Specify it manually.
linuxfb: Failed to initialize screen
Segmentation fault (core dumped)
I know the error might not be directly related to the board but I don't know where I'm supposed to debug in this situation.
It'd be really grateful if anyone can spot what's going on or suggest me where to debug.
Thank you.