Question from my customer, who has generated files with the PMT that should enable building a device tree. However, they are asking whether the generated files can be compiled to a .dtb file to startup Linux with the custom defined device tree.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Question from my customer, who has generated files with the PMT that should enable building a device tree. However, they are asking whether the generated files can be compiled to a .dtb file to startup Linux with the custom defined device tree.
Hi John,
By default the Linux build only builds the dtb/dtbo specified in Makefile.
The generated file content from PMT can either be copied in to existing dts file by updating main_pmx0 and wkup_pmx0 nodes or include the generated file in to existing dts file using (#include).
Regards,
Vishal