This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Processor IC request support peripherals with Wifi

Hi Team,

I would like to look for some help for our customer request for a Processor IC with the following requirements:
RAM 512MB/1GB ,SD Card, USB 2.0/3.0 , GSM/LTEM2 Modem ,DDR , WIFI (Linux OS)

Do we have something to offer because I am only seeing Sitara processor but it has no Wifi?
If ever the nearest possible is EVM, can you suggest one though the customer prefers an IC only

Thanks!

Jonathan.