This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NDK2.0 used in C6455 , Ping failed.

Our Board used LX971 as Phy chip.C6455 supply mac control.Download NDK2.0 and CSL for 6455 from ti web.

Edit example client.prj,compile,run.

As guide description,stout report:

TCP/IP Stack Example Client
Using MAC Address: 00-23-ae-9d-d3-04
 EMAC should be up and running 
EMAC has been started successfully
Registeration of the EMAC Successful
Link Status: 100Mb/s Full Duplex on PHY 1
Network Added: If-1:192.168.1.100
Service Status: Telnet   : Enabled  :          : 000
Service Status: HTTP     : Enabled  :          : 000

When ping target bord,it report : request time  out.

NDK version 2.0

NSP dsk6455

DSP c6455

PHY LX971

ccs version3.3

cable : direct net cable(2port as 568A standard)

hostip:192.168.1.1 gate:192.168.1.1 mask 255.255.255.0

bordip:192.168.1.100 gate:192.168.1.1 mask 255.255.255.0